Hi all,
i want to use the hard-float compiler arm-poky-linux-gnueabihf instead of the soft-float. how to setup the tool chain for this. So far i was able to use soft float and there isn't any examples for setting up hard-float compiler. below is my current build configuration
Build Configuration:
BB_VERSION = "1.26.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-14.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "wandboard-dual"
DISTRO = "poky"
DISTRO_VERSION = "1.8.1"
TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard cortexa9"
TARGET_FPU = "vfp-neon"
Could any one please tell me how to setup hard-float compiler, in my build directory i am only seeing arm-poky-linux-gnueabi which is the soft float compiler. Is there any specific instruction or configuration ? I am using wandboard-dual setup for testing.
已解决! 转到解答。
Hi Anjo,
what kernel are you using? Latest kernels use hard fp as default.
of you want to build an application please follow this syntax:
arm-poky-linux-gnueabi-gcc Test.c -mfloat-abi=hard -o test
Regards,
Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Anjo,
what kernel are you using? Latest kernels use hard fp as default.
of you want to build an application please follow this syntax:
arm-poky-linux-gnueabi-gcc Test.c -mfloat-abi=hard -o test
Regards,
Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------