using JPEG HW encoder on i.MX6Q under LTIB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

using JPEG HW encoder on i.MX6Q under LTIB

1,337件の閲覧回数
wolfgangt
Contributor I

Hi,

I want to use a jpeg library under linux that uses the hardware encoder/decoder on i.MX6Q.

Q: How do I select and use the proper library under LTIB?

Thanks!

As a side note:

- I have already tried to enable the jpeglib package with ltib config tool (./ltib -c)  but could not find any jpeg header file to inlcude

- also when I unzipped the package and looked into the documentation it was very general and did not have any specific reference to HW support

ラベル(2)
タグ(4)
0 件の賞賛
返信
1 返信

931件の閲覧回数
Yuri
NXP Employee
NXP Employee

The jpeglib is general  Linux package, which does not use hardware features of the i.MX6 VPU.

Please try the i.MX6 multimedia framework, linked below. In addition please refer to 

“i.MX_6Dual6Quad_VPU_API_Reference_Manual.pdf” in Linux documentation.


https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_MM_CODECS&appType=license&location=n...



https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_LINUX_MMDOCS&location=null&fpsp=1&Pa...

https://www.freescale.com/webapp/Download?colCode=L3.0.35_4.1.0_LINUX_DOCS&location=null&fpsp=1&Pare...

0 件の賞賛
返信