Hello everyone,
I am following i.MX 6 Q/D L3.0.35_1.1.0 GA release . I have an Element14 sabre-lite instead of one of the 3 boards that freescale offers.
I have downloaded the sources and docs and I am following the guide (found from L3.0.35_1.1.0_docs.tar.gz -> L3.0.35_1.1.0_docs -> L3.0.35_1.1.0_BSP_Documents -> SABRE_SD_User_Guide_L3.0.35_1.1.0.pdf )
I have extracted the L3.0.35_1.1.0_121218_source.tar.gz and installed LTIB running ./install.
I then move on to running
cd ltib
./ltib -m config.
However the process fails when building wget (from host_config.log)
gcc -O2 -Wall -Wno-implicit -o wget cmpt.o connect.o convert.o cookies.o ftp.o f
tp-basic.o ftp-ls.o ftp-opie.o hash.o headers.o host.o html-parse.o html-url.o h
ttp.o init.o log.o main.o gen-md5.o netrc.o progress.o rbuf.o recur.o res.o retr
.o safe-ctype.o snprintf.o gen_sslfunc.o url.o utils.o version.o -lssl -lcrypto
-ldl
gen_sslfunc.o: In function `init_ssl':
gen_sslfunc.c:(.text+0x343): undefined reference to `SSLv2_client_method'
collect2: ld returned 1 exit status
make[1]: *** [wget] Error 1
make[1]: Leaving directory `/opt/freescale/ltib/usr/src/rpm/BUILD/wget-1.9.1/src'
make: *** [src] Error 2
error: Bad exit status from /opt/slackaloo_nfs/freescale/ltib/tmp/rpm-tmp.73496 (%build)
RPM build errors:
Bad exit status from /opt/slackaloo_nfs/freescale/ltib/tmp/rpm-tmp.73496 (%build)
Build time for wget: 14 seconds
Failed building wget
Died at ./ltib line 1392.
traceback:
main::build_host_rpms:1392
main::host_checks:1447
main:554
The host is Linux mint 12.04.
I found that LTIB doesn't like ubuntu 12.04 ( ubuntu-ltib-patch.tgz ) , so I also tried removing the ltib directory, reinstalling, applying the patch and running ./ltib -m config once again. still no luck.
Anyone has seen this?
I read the LTIB "Failed building wget" undefined reference to `SSLv2_client_method' which refers to ubuntu 11.10 and imx53. So I was hoping the problem has been debuged since ubuntu 11.10....
Thank you for your help.
EDIT: actually ltib fails in other stages too. I re-deleted everything, re-extractred from the archive, patched again for ubuntu 12.04, and now it fails at
Processing: libtool
=====================
Processing: lkc
=================
Build path taken because: no prebuilt rpm,
Testing network connectivity
OK GPP:
Try lkc-1.4-lib.patch.md5 from the GPP
http://bitshrine.org/gpp//lkc-1.4-lib.patch.md5:
2013-05-09 17:35:38 ERROR 404: Not Found.
Try lkc-1.4-lib.patch from the GPP
http://bitshrine.org/gpp//lkc-1.4-lib.patch:
2013-05-09 17:35:38 ERROR 404: Not Found.
Can't get: lkc-1.4-lib.patch at ./ltib line 802.
Died at ./ltib line 1392.
traceback:
main::build_host_rpms:1392
main::host_checks:1447
main:554