user bitbake build system

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

user bitbake build system

899件の閲覧回数
2318516618
Contributor I

I use yocto build system,
Use the command:
DISTRO=fsl-imx-fb MACHINE=imx6ull14x14evk source imx-setup-release.sh -b build

Automatically enter the build folder and use the command:

bitbake imx-image-multimedia

But the linux-imx-headers-5.4-r0 file has not been found

   linux-imx-headers-5.4-r0 do_fetch - 1h57m28s

The following content is in the linux-imx-headers_5.4.bb file,is the download URL in this file wrong?

# Copyright 2017-2020 NXP
# Released under the MIT license (see COPYING.MIT for the terms)

SUMMARY = "Installs i.MX-specific kernel headers"
DESCRIPTION = "Installs i.MX-specific kernel headers to userspace. \
New headers are installed in ${includedir}/imx."
LICENSE = "GPLv2"
LIC_FILES_CHKSUM = "file://COPYING;md5=bbea815ee2795b2f4230826c0c6b8814"

SRCBRANCH = "imx_5.4.47_2.2.0"
LOCALVERSION = "-2.2.0"
KERNEL_SRC ?= "git://source.codeaurora.org/external/imx/linux-imx.git;protocol=https"
SRC_URI = "${KERNEL_SRC};branch=${SRCBRANCH}"

SRCREV = "dea2fede7e024ee7029b13e8d82a00ec14427777"


S = "${WORKDIR}/git"

do_compile[noexec] = "1"

IMX_UAPI_HEADERS = " \
dma-buf.h \
hantrodec.h \
hx280enc.h \
ion.h \
ipu.h \
isl29023.h \
mxc_asrc.h \
mxc_dcic.h \
mxc_mlb.h \
mxc_sim_interface.h \
mxc_v4l2.h \
mxcfb.h \
pxp_device.h \
pxp_dma.h \
videodev2.h \
"

do_install() {
# We install all headers inside of B so we can copy only the
# whitelisted ones, and there is no risk of a new header to be
# installed by mistake.
oe_runmake headers_install INSTALL_HDR_PATH=${B}${exec_prefix}

# FIXME: The ion.h is still on staging so "promote" it for now
cp ${S}/drivers/staging/android/uapi/ion.h ${B}${includedir}/linux

# Install whitelisted headers only
for h in ${IMX_UAPI_HEADERS}; do
install -D -m 0644 ${B}${includedir}/linux/$h \
${D}${includedir}/imx/linux/$h
done
}

ALLOW_EMPTY_${PN} = "1"

PACKAGE_ARCH = "${MACHINE_SOCARCH}"

 

 

0 件の賞賛
返信
1 返信

891件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

This url is correct, i think this should releate to your network environment.

https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_5.4.47_2.2.0

0 件の賞賛
返信