use mfgtool to upgrade rootfs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

use mfgtool to upgrade rootfs

1,296 Views
yufe
Contributor II

my custom board have mfg tool  to download firmware(have no ethernet port).I must use mfgtool to download whole rootfs even just modified only one file, it's a waste of time. Is there a convenient way to upgrade rootfs with mfgtool?

Tags (1)
0 Kudos
Reply
1 Reply

1,086 Views
art
NXP Employee
NXP Employee

Only the whole rootfs image can be reloaded with the MFGtool. If you only need to add a couple of files to your board's rootfs, better seems to use some external mass storage device, e.g. an USB Flash drive.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------