usbtty support in imx8 uboot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

usbtty support in imx8 uboot

跳至解决方案
1,336 次查看
vinayskumar
Contributor I

Is it possible to use USB as debug Port in imx8 u-boot and kernel?

 

One of our custom board based on iMX8QM CPU, the uart interfaces are not free for debug purpose.

So we are planning to use USB as the debug port. Will the latest u-boot will support it?

 

Regadrs

Vinay S

0 项奖励
回复
1 解答
1,330 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vinay

 

>So we are planning to use USB as the debug port. Will the latest u-boot will support it?

 

I am afraid not, additional customizations should be performed as described for example

on uboot mail list:

http://u-boot.10912.n7.nabble.com/how-to-support-usbtty-td44322.html

 

Best regards
igor

在原帖中查看解决方案

1 回复
1,331 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vinay

 

>So we are planning to use USB as the debug port. Will the latest u-boot will support it?

 

I am afraid not, additional customizations should be performed as described for example

on uboot mail list:

http://u-boot.10912.n7.nabble.com/how-to-support-usbtty-td44322.html

 

Best regards
igor