usbtty support in imx6 u-boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

usbtty support in imx6 u-boot

1,820 次查看
shabeerbadarudh
Contributor IV

Is it possible to use USB as debug Port in imx6 u-boot and kernel?

One of our custom project, the uart interfaces are not free for debug purpose.

So we are planning to use USB as the debug port. Will the latest u-boot will support it?

Regadrs

Shabeer

标签 (1)
0 项奖励
回复
2 回复数

1,326 次查看
art
NXP Employee
NXP Employee

Unfortunately, there is no usbtty support in u-boot for now.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,326 次查看
shabeerbadarudh
Contributor IV

Hi Artur,

Will it feasible to implement usbtty support in i.mx6 u-boot.

While refer the u-boot source, some borad configuration files contains  CONFIG_USB_TTY variable but we can not see console=ttyusb0 variable...

can we expect the imx6 u-boot will support ttyusb soon??

Thanks & Regards

Shabeer

0 项奖励
回复