usb otg detection issue in imx6dp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

usb otg detection issue in imx6dp

955件の閲覧回数
ssankar8
Contributor I

            We have a custom board with IMX6DP application processor. Trying to boot through Serial Downloader. But the USB OTG is not getting detected connected to pc. Boot mode is in serial downloader and asserting the reset. But the usb otg is not responding. Let me know the what could be wrong....

ラベル(1)
0 件の賞賛
返信
1 返信

874件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi saravana

reason may be poor usb traces layout (so signal is weak) or 24MHz crystal

instabilities, one can check board hardware using recommendations in

i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信