usb otg detection issue in imx6dp

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

usb otg detection issue in imx6dp

959 次查看
ssankar8
Contributor I

            We have a custom board with IMX6DP application processor. Trying to boot through Serial Downloader. But the USB OTG is not getting detected connected to pc. Boot mode is in serial downloader and asserting the reset. But the usb otg is not responding. Let me know the what could be wrong....

标签 (1)
0 项奖励
回复
1 回复

878 次查看
igorpadykov
NXP Employee
NXP Employee

Hi saravana

reason may be poor usb traces layout (so signal is weak) or 24MHz crystal

instabilities, one can check board hardware using recommendations in

i.MX6 System Development User’s Guide

https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复