we have been using uboot 2013.08 for long time. this is booted on HAB locked device. we are using scripts and cst BLN_CST_MAIN_02.03.00.
now I updated uboot to 2024.04. on unlocked device I get prints on consol.
same image if I sign with signing scripts its not booting on HAB locked device.
I see some difference in image with mkimage -l
OLD working image
Image Type: Freescale IMX Boot Image
Image Ver: 2 (i.MX53/6/7 compatible)
Mode: DCD
Data Size: 345088 Bytes = 337.00 KiB = 0.33 MiB
Load Address: 11ffb020
Entry Point: 12000000
HAB Blocks: 0x11ffb000 0x00000000 0x00052000
DCD Blocks: 0x00910000 0x0000002c 0x00000318
New image
Image Type: Freescale IMX Boot Image
Image Ver: 2 (i.MX53/6/7 compatible)
Mode: DCD
Data Size: 344064 Bytes = 336.00 KiB = 0.33 MiB
Load Address: 177ff420
Entry Point: 17800000
HAB Blocks: 0x177ff400 0x00000000 0x0004fc00
DCD Blocks: 0x00910000 0x0000002c 0x00000318
I am sure we are using correct keys to sign image.
any suggestion how to proceed ?