unable to mount the /dev/block/mmcblk0p1 in init.rc

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

unable to mount the /dev/block/mmcblk0p1 in init.rc

跳至解决方案
10,572 次查看
ManoharChinnadu
Contributor III

Here i'm doing the Board bringup activity and as of now able to bringup to kernel and fails to bringup AFS from the SD card.

 

I'm facing following issues:

1. Kernel is up and able to enter ramdisk.img(init.rc, init.freescale.rc..etc) but fail to mount with following command in init.freescale.rc

 

    mount vfat /dev/block/mmcblk0p1 /boot

    mount ext4 /dev/block/mmcblk0p5 /system

    # mount ext4 /dev/block/mmcblk0p5 /system ro remount

    mount ext4 /dev/block/mmcblk0p7 /data nosuid nodev nodiratime noatime noauto_da_alloc errors=panic

     mount ext4 /dev/block/mmcblk0p6 /cache nosuid nodev

    mount ext4 /dev/block/mmcblk0p8 /vendor nosuid nodev

 

2. with kernel and busybox i'm able to mount the card from by creating the mknod <filename> b 179 1  and able to access the partition.

 

3. from the kernel, we are able to detect the card from the kernel logs.

mmc1: host does not support reading read-only switch. assuming write-enable.

mmc1: new high speed SDHC card at address 0007

mmcblk0: mmc1:0007 SD04G 3.67 GiB

  mmcblk0: p1 p2 p3 < p5 p6 p7 p8 p9 > p4

 

4. please refer the logs file where i enabled the logs of kernel and init.rc file.

 

i have following Questions:

1. how to get the node file(/dev/block/mmcblk0p) is created or not when mmc driver is initialized  and block driver identified the partitions of sd card. because no access to shell to knw the details.

 

please give me your inputs regading this issue.

 

Original Attachment has been moved to: mount_fs.txt.zip

标签 (1)
1 解答
4,302 次查看
ManoharChinnadu
Contributor III

We fixed this issue by increasing the rootdelay timing by proving in boot arguments and now it's working fine without issues.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
4,302 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

hello Manohar Chinnadurai,

It seems strange in your SD partition table. Are you based on i.mx6+ ICS? But it seems different from our user guide does.

Can you list your SD partitions info?

0 项奖励
回复
4,303 次查看
ManoharChinnadu
Contributor III

We fixed this issue by increasing the rootdelay timing by proving in boot arguments and now it's working fine without issues.

0 项奖励
回复
4,302 次查看
oliver_chen
NXP Employee
NXP Employee

Good. I'm very glad to see that you can fix the issue by yourself.

0 项奖励
回复