Hi ,
As per the read me document in the IMX_Platform_SDK , Sourcery Codebench Lite toolchain is required to build the SDK. But I am not able to download the toolchain from any link . Could you please suggest me from where I can download the toolchain to build this SDK .
Regards,
Aditya Nagal
Hello Aditya Nagal,
You can use the link on the following thread:
Where to download Codebench Lite ARM EABI
Here is the link from the thread:
4.8-2014-q3-update : Series 4.8 : GNU ARM Embedded Toolchain
Alternatively you can use the Toolchain extracted from the BSP but it would required you to add the following settings when extracting it and it's much more straightforward using the recommended toolchain.
IMAGE_INSTALL_append = " eglibc-staticdev"
SDKIMAGE_FEATURES_append = " staticdev-pkgs"
I hope this helps!
Regards,