unable to connect wire for probe index 1 in while debuggine mimxrt1170

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

unable to connect wire for probe index 1 in while debuggine mimxrt1170

ソリューションへジャンプ
1,218件の閲覧回数
sandeep_c
Contributor I

unable to connect wire for probe index 1 in while debuggine mimxrt1170

iam getting the above error while debgging the rt1170evk board

i_MXRT1170Processor_0-1675322140714.png

 

0 件の賞賛
返信
1 解決策
1,204件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, 

I recommend reviewing the information on the page for the first use. Maybe need the external DC, it does not have an external DC please modify the power selection jumper or the boot source switch is wrong. The next link show, which is the USB for debugging, or if you are using an external debugger need an adapter to connect un the JTAG [J1].

Getting Started with the i.MX RT1170 Evaluation Kit | NXP Semiconductors

Best regards,
Pavel

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,205件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, 

I recommend reviewing the information on the page for the first use. Maybe need the external DC, it does not have an external DC please modify the power selection jumper or the boot source switch is wrong. The next link show, which is the USB for debugging, or if you are using an external debugger need an adapter to connect un the JTAG [J1].

Getting Started with the i.MX RT1170 Evaluation Kit | NXP Semiconductors

Best regards,
Pavel

0 件の賞賛
返信
1,200件の閲覧回数
sandeep_c
Contributor I
i boot the the rt1170 its working fine thanks for the reply
0 件の賞賛
返信