unable to bringup usb gadget in imx8m mini on USB1 interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

unable to bringup usb gadget in imx8m mini on USB1 interface

跳至解决方案
1,446 次查看
jigar2
Contributor II

I'm trying to bring up a custom board with iMX8M mini processor with 32bit LPDDR4 RAM, Where i'm able to bring up the uboot using SDP mode by setting boot in Serial Download and trying to use boot linux kernel using uuu script. Here i'm trying to to use RAMDISK in kernel so no need to flash emmc.
while trying to bring up USB on USB1 i'm getting No USB device found USB init failed: -19 Here i've attached all my changes. If anyone point me to specific area where to troubleshoot further. We have removed type c port from code as we are not using the one.

I'm using u-boot from branch lf_v2022.04 and kernel from branch lf-5.15.71-2.2.0.

UUU script

 

uuu_version 1.5.165


# Please Replace below items with actually file names
# @_flash.bin            		| boot loader
# @_Image            			| kernel image, arm64 is Image, arm32 it is zImage
# @_board.dtb            		| board dtb file
# @_initramfs.cpio.gz.uboot    		| mfgtool init ramfs
# @_rootfs.tar.bz2        		| rootfs
# @_uTee.tar            		| optee image, put dummy _uTee.tar file here if platform is not MX6/MX7*

# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ
SDP: boot -f imx-boot.bin

# This command will be run when ROM support stream mode
# i.MX8QXP, i.MX8QM
SDPS[-t 10000]: boot -f imx-boot.bin

# These commands will be run when use SPL and will be skipped if no spl
# SDPU will be deprecated. please use SDPV instead of SDPU
# {
SDPU: delay 1000
SDPU: write -f imx-boot.bin -offset 0x57c00
SDPU: jump
#SDPU: done
# }

# These commands will be run when use SPL and will be skipped if no spl
# if (SPL support SDPV)
# {
SDPV: delay 1000
SDPV: write -f imx-boot.bin -skipspl
SDPV: jump
#SDPV: done
# }

# use uboot burn bootloader to eMMC
# becaue difference chip, offset is difference
# you can use kernel to do that for specific boards
FB: ucmd setenv fastboot_dev mmc
FB: ucmd setenv mmcdev ${emmc_dev}

FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;

FB: ucmd setenv emmc_cmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0
FB: ucmd if test "${emmc_skip_fb}" != "yes"; then run emmc_cmd; fi
FB: ucmd setenv emmc_cmd mmc bootbus ${emmc_dev} 2 2 1;
FB: ucmd if test "${emmc_skip_fb}" != "yes"; then run emmc_cmd; fi

FB: ucmd setenv fastboot_buffer ${loadaddr}
FB: download -f Image
FB: ucmd setenv fastboot_buffer ${fdt_addr}
FB: download -f imx8mm-mez.dtb
FB: ucmd setenv fastboot_buffer ${initrd_addr}
FB: download -f rootfs-overlay-initramfs-imx8mm-mez-20240403050131.rootfs.cpio.gz
#FB: ucmd setenv bootargs console=${console},${baudrate} earlycon=${earlycon},${baudrate}
FB: acmd ${kboot} ${loadaddr} ${initrd_addr} ${fdt_addr}

 

 

Boot log

 

 

U-Boot SPL 2022.04-dirty (Apr 11 2024 - 12:50:52 +0530)                                                                 
power_bd71837_init                                                                                                      
DDRINFO: start DRAM init                                                                                                
DDRINFO: DRAM rate 3000MTS                                                                                              
DDRINFO:ddrphy calibration done                                                                                         
DDRINFO: ddrmix config done                                                                                             
SEC0:  RNG instantiated                                                                                                 
Normal Boot                                                                                                             
Trying to boot from USB SDP                                                                                             
board_usb_init 0, type 1                                                                                                
SDP: initialize...                                                                                                      
SDP: handle requests...                                                                                                 
Downloading file of size 1303888 to 0x40400000... done                                                                  
Jumping to header at 0x40400000                                                                                         
Header Tag is not an IMX image                                                                                          
Found header at 0x40427fa0                                                                                              
board_usb_cleanup 0, type 1                                                                                             
NOTICE:  BL31: v2.6(release):lf-6.1.1-1.0.0-0-g616a4588f-dirty                                                          
NOTICE:  BL31: Built : 06:16:04, Apr  4 2024                                                                            
                                                                                                                        
                                                                                                                        
U-Boot 2022.04-dirty (Apr 11 2024 - 12:50:52 +0530)                                                                     
                                                                                                                        
CPU:   i.MX8MMS rev1.0 1800 MHz (running at 1200 MHz)                                                                   
CPU:   Commercial temperature grade (0C to 95C) at 58C                                                                  
Reset cause: POR                                                                                                        
Model: Silmates i.MX8MM SoM board                                                                                       
DRAM:  512 MiB                                                                                                          
Core:  73 devices, 25 uclasses, devicetree: separate                                                                    
MMC:   FSL_SDHC: 1, FSL_SDHC: 2                                                                                         
Loading Environment from MMC... *** Warning - bad CRC, using default environment                                        
                                                                                                                        
[*]-Video Link 0probe video device failed, ret -2                                                                       
                                                                                                                        
        [0] lcdif@32e00000, video                                                                                       
        [1] mipi_dsi@32e10000, video_bridge                                                                             
        [2] adv7535@3d, panel                                                                                           
probe video device failed, ret -2                                                                                       
In:    serial                                                                                                           
Out:   serial                                                                                                           
Err:   serial                                                                                                           
SEC0:  RNG instantiated                                                                                                 
                                                                                                                        
 BuildInfo:                                                                                                             
  - ATF 616a458                                                                                                         
                                                                                                                        
switch to partitions #0, OK                                                                                             
mmc2(part 0) is current device                                                                                          
Detect USB boot. Will enter fastboot mode!                                                                              
Net:                                                                                                                    
Warning: ethernet@30be0000 (eth0) using random MAC address - 92:85:f8:75:c0:7f                                          
eth0: ethernet@30be0000                                                                                                 
Fastboot: Normal                                                                                                        
Boot from USB for mfgtools                                                                                              
*** Warning - Use default environment for                                mfgtools                                       
, using default environment                                                                                             
                                                                                                                        
Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_a
ddr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;  
Hit any key to stop autoboot:  0                                                                                        
                                                                                                                        
## Checking Image at 43800000 ...                                                                                       
Unknown image format!                                                                                                   
Run fastboot ...                                                                                                        
controller_index : 0                                                                                                    
No USB device found                                                                                                     
USB init failed: -19                                                                                                    
u-boot=> usb start                                                                                                      
starting USB...                                                                                                         
Bus usb@32e40000: board_usb_init 0, type 0                                                                              
Port not available.                                                                                                     
u-boot=> 

 

 

usb initialization in board.c

 

int board_usb_init(int index, enum usb_init_type init)
{
	int ret = 0;

	printf("board_usb_init %d, type %d\n", index, init);

	imx8m_usb_power(index, true);

	return ret;
}

int board_usb_cleanup(int index, enum usb_init_type init)
{
	int ret = 0;

	printf("board_usb_cleanup %d, type %d\n", index, init);

	imx8m_usb_power(index, false);
	return ret;
}
int board_ehci_usb_phy_mode(struct udevice *dev)
{
    printf("........ board_ehci_usb_phy_mode comein %d \n",dev->seq_);
	return USB_INIT_DEVICE;
}

 

 

 device tree settings in uboot

 

&usbotg1 {
	dr_mode = "otg";
	status = "okay";
};

&usbotg2 {
	status = "disabled";
};

 

 

default defconfig for usb in uboot

 

 

CONFIG_CMD_USB=y
CONFIG_CMD_USB_MASS_STORAGE=y
CONFIG_CMD_USB_SDP=y
CONFIG_USB_FUNCTION_FASTBOOT=y
CONFIG_USB_TCPC=n
CONFIG_USB=y
CONFIG_USB_GADGET=y
CONFIG_USB_STORAGE=y
CONFIG_DM_USB=y
CONFIG_USB_EHCI_HCD=y
CONFIG_USB_HOST_ETHER=y
CONFIG_USB_ETHER_ASIX=y
CONFIG_USB_ETHER_RTL8152=y
CONFIG_USB_GADGET_DOWNLOAD=y
CONFIG_USB_GADGET_MANUFACTURER="FSL"
CONFIG_USB_GADGET_VENDOR_NUM=0x1fc9
CONFIG_USB_GADGET_PRODUCT_NUM=0x0152
CONFIG_FASTBOOT_USB_DEV=0
CONFIG_SPL_USB_HOST=y
CONFIG_SPL_USB_GADGET=y
CONFIG_SPL_USB_SDP_SUPPORT=y

 

 

 

标签 (2)
0 项奖励
回复
1 解答
1,408 次查看
jigar2
Contributor II

Got solution

Who ever want to port u-boot for custom board consider board-u-boot.dtsi file u-boot consider this file without mentioning in Makefile.

Below is the link which describe the functionality of xxx-u-boot.dtsi.

https://community.nxp.com/t5/i-MX-Processors/What-is-the-purpose-of-imx8mn-evk-u-boot-dtsi/m-p/18389...

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,409 次查看
jigar2
Contributor II

Got solution

Who ever want to port u-boot for custom board consider board-u-boot.dtsi file u-boot consider this file without mentioning in Makefile.

Below is the link which describe the functionality of xxx-u-boot.dtsi.

https://community.nxp.com/t5/i-MX-Processors/What-is-the-purpose-of-imx8mn-evk-u-boot-dtsi/m-p/18389...

0 项奖励
回复