ui and video combining on imx6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ui and video combining on imx6q

Jump to solution
5,498 Views
xiehuijun
Contributor II

hello everyone, i have some trouble in imx6q about ui and video combining.

i'm using buildroot for system (kernel 3.10 + QT5.5 + eglfs2.0 ). i want to play video and show transparent picture(eg: png) on the top of video.

my kernel boot args:"video=mxcfb0:dev=hdmi,1920x1080@60,if=RGB24,bpp=32 "

i have try some methods like this :

set video output to "video16"(BG),and set QT output to "fb1"(FG), this can work, but the background of "fb1" is not transparent and "fb1" have covered the video.

i tried to set the background of qt widget to transparent and set the "alpha"and"color_key" of fb1 device,  but no effect both,or the settings is wrong ?

i also tried to set video output to "video16"(BG),and set QT output to "fb0"(BG), it will just show video only.

i can't find any demos for this, is there any method for my purpose ?

i'm look forward to you, thanks.

Labels (3)
0 Kudos
Reply
1 Solution
4,618 Views
xiehuijun
Contributor II

the packet i used is at version 3.10.53, and at this version, the gstreamer-0.10 can not solve my problem. i must use gstreamer-1.0. now, i can draw transparent pictures on video and it looks perfect. thanks anyway, i wish this discussion can help someone else.

View solution in original post

0 Kudos
Reply
11 Replies
4,617 Views
yyuan
Contributor III

please

i have the same problem whth you?   how to slove it? 

please help me 

thank you

0 Kudos
Reply
4,617 Views
joanxie
NXP TechSupport
NXP TechSupport

"the background of "fb1" is not transparent",do you mean fb0?

and how did you set the transparent? you couldnt' find any difference after you set the parameter?

0 Kudos
Reply
4,617 Views
xiehuijun
Contributor II

Supplementary description:

the fb1 device is not as 1920x1080@60 resolution after kernel start up.

# fbset -s -fb /dev/fb0

mode "1920x1080-60"

        # D: 148.500 MHz, H: 67.500 kHz, V: 60.000 Hz

        geometry 1920 1080 1920 1080 32

        timings 6734 148 88 36 4 44 5

        accel false

        rgba 8/16,8/8,8/0,8/24

endmode

#

# fbset -s -fb /dev/fb1

mode "240x320-60"

        # D: 4.608 MHz, H: 19.200 kHz, V: 60.000 Hz

        geometry 240 320 240 960 16

        timings 217013 0 0 0 0 0 0

        accel false

        rgba 5/11,6/5,5/0,0/0

endmode

#

i try to set fb1 to the same as fb0 like this:

     struct fb_var_screeninfo var;

    /* set fb1  */

    ret = ioctl( fd_fb0, FBIOGET_VSCREENINFO, &var );

    if( ret < 0 ){

        printf( "ioctl %s FBIOGET_VSCREENINFO failed\n", fb_dev_path[FB_0] );

        goto err;

    }

    var.activate = FB_ACTIVATE_FORCE;

    ret = ioctl( fd_fb1, FBIOPUT_VSCREENINFO, &var );

    if( ret < 0 ){

        printf( "ioctl %s FBIOPUT_VSCREENINFO failed\n", fb_dev_path[FB_1] );

        goto err;

    }

is there any demos or documents about UI and video mixing ?

0 Kudos
Reply
4,616 Views
joanxie
NXP TechSupport
NXP TechSupport

Here is an example to config frame buffer for alpha in pixel  function, you can have a try.

retval = ioctl(fd, FBIOGET_VSCREENINFO, &fb_var);
if (retval < 0)
{
       printf("fb ioctl FBIOGET_VSCREENINFO fail\n");
}

fb_var.xres = 1280;
fb_var.yres = 720;
fb_var.bits_per_pixel = 32;
fb_var.activate |= FB_ACTIVATE_FORCE;
fb_var.nonstd = v4l2_fourcc('A', 'B', 'G', 'R');
fb_var.red.offset = 24;
fb_var.red.length = 8;
fb_var.green.offset = 16;
fb_var.green.length = 8;
fb_var.blue.offset = 8;
fb_var.blue.length = 8;
fb_var.transp.offset = 0;
fb_var.transp.length = 8;

fb_var.xres_virtual = fb_var.xres;
fb_var.yres_virtual = fb_var.yres * 3;
fb_var.yoffset = 0;

retval = ioctl(fd, FBIOPUT_VSCREENINFO, &fb_var);
if (retval < 0)
{
       printf("fb ioctl FBIOPUT_VSCREENINFO fail\n");
}

loc_alpha.enable = 1;
loc_alpha.alpha_in_pixel = 1;
retval = ioctl(fd, MXCFB_SET_LOC_ALPHA, &loc_alpha);
if (retval < 0)
{
       printf("fb ioctl MXCFB_SET_LOC_ALPHA fail\n");
}
ioctl(fd, MXCFB_WAIT_FOR_VSYNC, 0);
ioctl(fd, FBIOBLANK, FB_BLANK_UNBLANK);

0 Kudos
Reply
4,617 Views
xiehuijun
Contributor II

i tried, it doesn't work!, the background is red now, not transparent.

thanks.

0 Kudos
Reply
4,617 Views
joanxie
NXP TechSupport
NXP TechSupport

this is example code, did you change it based on your case(like pixel format)? if yes, pls share your code, let's check it.

0 Kudos
Reply
4,619 Views
xiehuijun
Contributor II

the packet i used is at version 3.10.53, and at this version, the gstreamer-0.10 can not solve my problem. i must use gstreamer-1.0. now, i can draw transparent pictures on video and it looks perfect. thanks anyway, i wish this discussion can help someone else.

0 Kudos
Reply
4,617 Views
xiehuijun
Contributor II

thanks for reminding me modify your sample code.

this is part of my code below:

     retval = ioctl(fb1, FBIOGET_VSCREENINFO, &fb_var);

    ...

     fb_var.xres = 1920;

    fb_var.yres = 1080;

    fb_var.bits_per_pixel = 32;

    fb_var.activate |= FB_ACTIVATE_FORCE;

    fb_var.nonstd = v4l2_fourcc('B', 'G', 'R','A');

    fb_var.red.offset = 16;

    fb_var.red.length = 8;

    fb_var.green.offset = 8;

    fb_var.green.length = 8;

    fb_var.blue.offset = 0;

    fb_var.blue.length = 8;

    fb_var.transp.offset = 24;

    fb_var.transp.length = 8;

    fb_var.xres_virtual = fb_var.xres;

    fb_var.yres_virtual = fb_var.yres * 3;

    fb_var.yoffset = 0;

    retval = ioctl(fb1, FBIOPUT_VSCREENINFO, &fb_var);

     ...

     loc_alpha.enable = 1;

    loc_alpha.alpha_in_pixel = 1;

    retval = ioctl(fb1, MXCFB_SET_LOC_ALPHA, &loc_alpha);

    ...

    ioctl(fb1, MXCFB_WAIT_FOR_VSYNC, 0);

    ioctl(fb1, FBIOBLANK, FB_BLANK_UNBLANK);

after running this code, the background is black still.

the fb1 settings is :

# fbset -fb /dev/fb1 -s

mode "1920x1080-2"

        # D: 4.608 MHz, H: 2.400 kHz, V: 2.222 Hz

        geometry 1920 1080 1920 2160 32

        timings 217013 0 0 0 0 0 0

        accel false

        rgba 8/16,8/8,8/0,8/24

endmode

#

and some settings of fb0 is changed.

before running, the settings of fb0 is :

# fbset -s -fb /dev/fb0

mode "1920x1080-60"

        # D: 148.500 MHz, H: 67.500 kHz, V: 60.000 Hz

        geometry 1920 1080 1920 1080 32

        timings 6734 148 88 36 4 44 5

        accel false

        rgba 8/16,8/8,8/0,8/24

endmode

#

after, it is :

# fbset -fb /dev/fb0 -s

mode "1920x1080-60"

        # D: 148.500 MHz, H: 67.500 kHz, V: 60.000 Hz

        geometry 1920 1080 1920 3240 16

        timings 6734 148 88 36 4 44 5

        accel false

        rgba 5/11,6/5,5/0,0/0

endmode

#

the "bpp" ,"vyres" "rgba" is changed .

i also tried to copy all settings of fb0 to fb1, it worked the same.

0 Kudos
Reply
4,617 Views
xiehuijun
Contributor II

"the background of "fb1" is not transparent" means there is  a black background on the top of video, even though i set the background of qt window to transparent.

for example:

i want to show a qt window (which draw a png picture )on the top of video, but actually the background of window is black.

i set the background of qt window to transparent with this code :

"

void MainWindow::paintEvent(QPaintEvent *e)

{

    QPainter p(this);

    p.setCompositionMode( QPainter::CompositionMode_Clear );

    p.fillRect( this->rect(), Qt::SolidPattern );

}

"

i also tried this:

QPalette pal = palette();

pal.setColor(QPalette::Background, QColor(0x00,0x00,0x00,0x00));//

setPalette(pal);

but no effect,the background of window is also black.

at the internet, i find some way (setting the alpha and color_key of fb device )like this:

    int fd = 0,ret = 0;

    struct mxcfb_gbl_alpha gbl_alpha;

    gbl_alpha.alpha = 0;

    gbl_alpha.enable = 1;

    if ((fd = open("/dev/fb1", O_RDWR)) < 0){

        printf("Unable to open /dev/fb1 !!!\n");

        return;

    }

    ret = ioctl(fd, MXCFB_SET_GBL_ALPHA, &gbl_alpha);

    if(ret <0) {

        printf("Error!MXCFB_SET_GBL_ALPHA failed!");

        return;

    }

    struct mxcfb_color_key key;

    key.enable = 1;

    key.color_key = 0x00000000; // Black

    ret = ioctl(fd, MXCFB_SET_CLR_KEY, &key);

    if(ret <0) {

        printf("Error!Colorkey setting failed for dev ");

        return;

    }

but also no effect,and will take some errors about IPU sometime.

is the imx6q platform not support this function  or need some patches?

thanks a lot

0 Kudos
Reply
4,617 Views
joanxie
NXP TechSupport
NXP TechSupport

I found a topic for transparent window on qt, hope helpful for you

[solved] how to get an simple transparent window | Qt Forum

0 Kudos
Reply
4,617 Views
xiehuijun
Contributor II

i have tried this approach from the link "[solved] how to get an simple transparent window | Qt Forum" you told me, but it doesn't work.

i think the problem can not be solved by QT only, because it related to mix of two framebuffers. it should depend on IMX6Q platform.

the key is that there is no demo or doc about this. i have touched to the FAE of freescale, they hav't replied yet.

thanks again.

0 Kudos
Reply