ubuntu prebuilt image for mx6sabresd board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ubuntu prebuilt image for mx6sabresd board

416 Views
sachusanal
Contributor III

Dear Sir ,

Could you please give me the ubuntu prebuilt image for imx6qsabresd board(Evaluation kit)

please share with me tha image its urgent

Labels (1)
0 Kudos
1 Reply

307 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi sachu sanal,

In freescale website you can download L3.0.35_4.1.0_UBUNTU_RFS_BSP, which is the Linux File System for the Ubuntu Images. About the u-boot and kernel you have to build yourself. The link is :SABRE for Smart Devices Reference Design|Freescale .

Here could you tell me which version of BSP are you using?
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos