ubuntu 21.10 upgrade on imx-5.10.72-2.2.0_desktop.xml

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ubuntu 21.10 upgrade on imx-5.10.72-2.2.0_desktop.xml

2,082件の閲覧回数
yueningliu
Contributor I

Hi, all

For a ubuntu desktop, I use imx-5.10.72-2.2.0_desktop.xml branch on https://source.codeaurora.org/external/imx/imx-manifest/?h=imx-linux-hardknott.

Because I want to use gnome 40, so I decide to upgrade to ubuntu 21.10,  but I am a freshman for yocto project, I made some modification as following:

 

project sources/meta-nxp-desktop/
diff --git a/conf/distro/imx-desktop-xwayland.conf b/conf/distro/imx-desktop-xwayland.conf
index a921118..f1f8c89 100644
--- a/conf/distro/imx-desktop-xwayland.conf
+++ b/conf/distro/imx-desktop-xwayland.conf
@@ -28,7 +28,7 @@ PREFERRED_VERSION_qemu-native = "4.2.1"
PREFERRED_VERSION_qemu = "4.2.1"

GCCVERSION = "9.3.0"
-GLIBCVERSION = "2.31%"
+GLIBCVERSION = "2.34%"

IMX_GPU_VERSION = "6.4.3.p2.4d"

diff --git a/conf/machine/include/ubuntubasics.inc b/conf/machine/include/ubuntubasics.inc
index fddee2e..a7f6abe 100644
--- a/conf/machine/include/ubuntubasics.inc
+++ b/conf/machine/include/ubuntubasics.inc
@@ -3,7 +3,8 @@
# - 18.04.3
#UBUNTU_TARGET_VERSION ?= "16.04.5"
#UBUNTU_TARGET_VERSION ?= "18.04.3"
-UBUNTU_TARGET_VERSION ?= "20.04.3"
+#UBUNTU_TARGET_VERSION ?= "20.04.3"
+UBUNTU_TARGET_VERSION ?= "21.10"

UBUNTU_TARGET_MAJORVERSION ?= "${@d.getVar('UBUNTU_TARGET_VERSION', True).rsplit('.')[0]}"
UBUNTU_TARGET_MINORVERSION ?= "${@d.getVar('UBUNTU_TARGET_VERSION', True).rsplit('.')[1]}"
@@ -39,9 +40,11 @@ GLIBCVERSION = '${@ \
oe.utils.conditional("UBUNTU_TARGET_BASEVERSION", "16.04", "2.23", \
oe.utils.conditional("UBUNTU_TARGET_BASEVERSION", "18.04", "2.27", \
oe.utils.conditional("UBUNTU_TARGET_BASEVERSION", "20.04", "2.31%", \
+ oe.utils.conditional("UBUNTU_TARGET_BASEVERSION", "21.10", "2.34%", \
"unsupportedubuntuversion" \
, d) \
, d) \
+ , d) \
, d)}'
PREFERRED_VERSION_cross-localedef-native = "${GLIBCVERSION}"
BINUVERSION="2.34"
@@ -52,7 +55,9 @@ DISTRO_FEATURES_append = '${@ \
oe.utils.conditional("UBUNTU_TARGET_BASEVERSION", "16.04", "", \
oe.utils.conditional("UBUNTU_TARGET_BASEVERSION", "18.04", "", \
oe.utils.conditional("UBUNTU_TARGET_BASEVERSION", "20.04", " usrmerge", \
+ oe.utils.conditional("UBUNTU_TARGET_BASEVERSION", "21.10", " usrmerge", \
"unsupportedubuntuversion" \
+ , d) \
, d) \
, d) \
, d)}'
diff --git a/recipes-extended/ubuntu/ubuntu-base_20.04.3.bb b/recipes-extended/ubuntu/ubuntu-base_20.04.3.bb
index 7d89ef8..08cacc9 100644
--- a/recipes-extended/ubuntu/ubuntu-base_20.04.3.bb
+++ b/recipes-extended/ubuntu/ubuntu-base_20.04.3.bb
@@ -3,8 +3,10 @@ require ubuntu-license.inc
SECTION = "devel"

# Desktop 20.04.2 baseline
-SRC_URI[md5sum] = "b39023c9ed58323c2bb3c324569cff20"
-SRC_URI[sha256sum] = "e54a49b3f5bc1a4242167a3270d0648cabfb9c02b9a59b7a28a860a9b721cde1"
+#SRC_URI[md5sum] = "b39023c9ed58323c2bb3c324569cff20"
+SRC_URI[md5sum] = "b58b9b3d7476184b0514e3770679867c"
+#SRC_URI[sha256sum] = "e54a49b3f5bc1a4242167a3270d0648cabfb9c02b9a59b7a28a860a9b721cde1"
+SRC_URI[sha256sum] = "86cdcd2beca9aa34b6c0334cd055ddaa3433750e71224cf4c07282e5aa3c8c2a"

require ubuntu-base.inc

diff --git a/recipes-fsl/images/imx-image-desktop.bb b/recipes-fsl/images/imx-image-desktop.bb
index 7979d14..dfd1d77 100644
--- a/recipes-fsl/images/imx-image-desktop.bb
+++ b/recipes-fsl/images/imx-image-desktop.bb
@@ -51,11 +51,13 @@ IMAGE_INSTALL += "\
clutter-gst-3.0 \
cheese \
xserver-xorg-xwayland \
- chromium-ozone-wayland \
tensorflow-lite \
${ML_NNSTREAMER_PKGS} \
armnn \
"
+
+# chromium-ozone-wayland
+#
# We want to have an itb to boot from in the /boot directory to be flexible
# about U-Boot behavior
#IMAGE_INSTALL += "\

 

after my mading a compilation, I got the following ERROR:

 

ERROR: imx-image-desktop-21.10-r0 do_rootfs: Could not invoke dnf. Command '/data/ynliu/imx-yocto-bsp/build-desktop/tmp/work/imx8mpevk-fsl-linux/imx-image-desktop/21.10-r0/recipe-sysroot-native/usr/bin/dnf -v --rpmverbosity=info -y -c /data/ynliu/imx-yocto-bsp/build-desktop/tmp/work/imx8mpevk-fsl-linux/imx-image-desktop/21.10-r0/rootfs/etc/dnf/dnf.conf --setopt=reposdir=/data/ynliu/imx-yocto-bsp/build-desktop/tmp/work/imx8mpevk-fsl-linux/imx-image-desktop/21.10-r0/rootfs/etc/yum.repos.d --installroot=/data/ynliu/imx-yocto-bsp/build-desktop/tmp/work/imx8mpevk-fsl-linux/imx-image-desktop/21.10-r0/rootfs --setopt=logdir=/data/ynliu/imx-yocto-bsp/build-desktop/tmp/work/imx8mpevk-fsl-linux/imx-image-desktop/21.10-r0/temp --repofrompath=oe-repo,/data/ynliu/imx-yocto-bsp/build-desktop/tmp/work/imx8mpevk-fsl-linux/imx-image-desktop/21.10-r0/oe-rootfs-repo --nogpgcheck install alsa-state apitrace armnn basler-camera cheese clutter-gst-3.0 firmware-imx-easrc-imx8mn firmware-imx-sdma-imx7d firmware-imx-xcvr-imx8mp firmwared gputop imx-alsa-plugins imx-g2d-samples imx-gpu-viv-tools imx-m7-demos isp-imx kernel-devicetree kernel-image kernel-module-isp-vvcam kernel-module-nxp89xx kernel-modules libclc-imx libclc-imx-dev libcogl libdrm-vivante libegl-imx libegl-imx-dev libgal-imx libgal-imx-dev libgbm-imx libgbm-imx-dev libgles1-imx libgles1-imx-dev libgles2-imx libgles2-imx-dev libgles3-imx-dev libglslc-imx libgpuperfcnt libnn-imx libopencl-imx libopenvx-imx libopenvx-imx-dev libvsc-imx libvulkan-imx linux-firmware-ath10k linux-firmware-nxp89xx nnshark nnstreamer nnstreamer-protobuf nnstreamer-python3 nnstreamer-tensorflow-lite nxp-wlan-sdk packagegroup-fsl-gstreamer1.0 packagegroup-fsl-gstreamer1.0-full perf sof-imx systemd-gpuconfig tensorflow-lite ubuntu-base ubuntu-base-dbg ubuntu-base-dev ubuntu-base-doc udev-rules-imx wayland-protocols xserver-xorg-xwayland' returned 1:
DNF version: 4.6.0
cachedir: /data/ynliu/imx-yocto-bsp/build-desktop/tmp/work/imx8mpevk-fsl-linux/imx-image-desktop/21.10-r0/rootfs/var/cache/dnf
Added oe-repo repo from /data/ynliu/imx-yocto-bsp/build-desktop/tmp/work/imx8mpevk-fsl-linux/imx-image-desktop/21.10-r0/oe-rootfs-repo
User-Agent: falling back to 'libdnf': could not detect OS or basearch
repo: using cache for: oe-repo
oe-repo: using metadata from Fri 28 Jan 2022 08:35:13 AM UTC.
Last metadata expiration check: 0:00:01 ago on Fri 28 Jan 2022 08:35:13 AM UTC.
--> Starting dependency resolution
--> Finished dependency resolution
Error:
Problem 1: conflicting requests
- nothing provides ubuntu-base = 21.10 needed by isp-imx-4.2.2.16.0d-r0.cortexa53_crypto_mx8mp
Problem 2: conflicting requests

..................

 

I suspect that the glibc version lead to the problem, I have no too much ideas to it, any suggestion or help

is welcome.

Thanks in advance

 

0 件の賞賛
返信
1 返信

2,055件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello yueningliu,

We haven't tested the ubuntu 21.10 but you can access to 20.04 ubuntu BSP:

https://source.codeaurora.org/external/imx/meta-nxp-desktop/tree/README.md?h=imx-5.10.72-hardknott

Regards

 

0 件の賞賛
返信