ubuntu 14.04 uuu tool issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ubuntu 14.04 uuu tool issue

3,898 次查看
zhaocq
Contributor II

ubuntu 14.04 using uuu tool to download images encounter the below error, it seems tools can not find uuu. Could you tell me how to install uuu, i have download uuu attached file?

root@zhaocq-Lenovo:/home/zhaocq/imx8qm_mek/android_p9.0.0_2.1.0-auto-ga_image_8qmek# ./uuu_imx_android_flash.sh -f imx8qm
This script is validated with uuu 1.2.91 version, please align with this version.
dual bootloader is supported
dtbo is supported
dual slot is supported
generate lines to flash partition-table.img to the partition of gpt
generate lines to flash spl-imx8qm.bin to the partition of bootloader0
generate lines to flash bootloader-imx8qm.img to the partition of bootloader_a
generate lines to flash dtbo-imx8qm.img to the partition of dtbo_a
generate lines to flash boot.img to the partition of boot_a
generate lines to flash system.img to the partition of system_a
generate lines to flash vendor.img to the partition of vendor_a
generate lines to flash vbmeta-imx8qm.img to the partition of vbmeta_a
generate lines to flash bootloader-imx8qm.img to the partition of bootloader_b
generate lines to flash dtbo-imx8qm.img to the partition of dtbo_b
generate lines to flash boot.img to the partition of boot_b
generate lines to flash system.img to the partition of system_b
generate lines to flash vendor.img to the partition of vendor_b
generate lines to flash vbmeta-imx8qm.img to the partition of vbmeta_b
uuu script generated, start to invoke uuu with the generated uuu script
./uuu_imx_android_flash.sh: 行 524: uuu: 未找到命令

0 项奖励
回复
4 回复数

2,794 次查看
edwardtyrrell
Senior Contributor I

Hi, 

Looks like your original question has not been answered.. How to get uuu, check this link: https://emteria.com/kb/uuu-linux  The link will also show you how to add uuu to your path so the uuu_imx_andriod_flash.sh will find it. Check in a terminal by simply typing uuu (return/enter). You may have an issue with 14.04 it is quite old; recently I was forced to get another machine on 20.04 to use modern tools. Hope this helps..

 

 

0 项奖励
回复

3,610 次查看
zhaocq
Contributor II

Thanks for your reply, it's ok

0 项奖励
回复

3,610 次查看
joanxie
NXP TechSupport
NXP TechSupport

you need add your uuu path in the command, the simple solution is that add "./" before "uuu" in the 524 lines of uuu_imx_android_flash.sh

0 项奖励
回复

2,808 次查看
Kusuma
Contributor II

Im also facing same issue.

i have added the path also using ./ but still i have error

/android-12.0.0_1.0.0_image_8mmevk$ sudo ./uuu_imx_android_flash.sh -f imx8mm -a -e -u trusty
This script is validated with uuu 1.4.182 version, it is recommended to align with this version.
dtbo is supported
dual slot is supported
dynamic parttition is supported
vendor_boot parttition is supported
generate lines to flash u-boot-imx8mm-trusty.imx to the partition of bootloader0
generate lines to flash partition-table.img to the partition of gpt
generate lines to flash dtbo-imx8mm.img to the partition of dtbo_a
generate lines to flash boot.img to the partition of boot_a
generate lines to flash vendor_boot.img to the partition of vendor_boot_a
generate lines to flash vbmeta-imx8mm.img to the partition of vbmeta_a
generate lines to flash super.img to the partition of super
uuu script generated, start to invoke uuu with the generated uuu script
./uuu_imx_android_flash.sh: line 758: uuu: command not found

0 项奖励
回复