uboot prompt is not getting in imx6dl Oreo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uboot prompt is not getting in imx6dl Oreo

1,023件の閲覧回数
vivektol
Contributor I

Hi All,

          I have imx6dl custom board with 2GB DDR3 RAM.

I have customized ram in oreo uboot-imx.

When I boot the board, I am not getting "Hit any key to stop Autoboot" message.

Directly kernel is booting and I am getting Kernel Prompt.

 I want uboot prompt to change HDMI boot argument.

else

where can I fixed uboot arguments for HDMI in uboot-imx source code ?

Please help me.

With Regards,

VIVEK TOL

ラベル(6)
0 件の賞賛
返信
1 返信

924件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi VIVEK

one can check "bootargs" arguments in uboot/include/configs/mx6sabre_common.h
uboot-imx.git - Freescale i.MX u-boot Tree 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信