uboot loads the kernel from emmc ont the imx8mp

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

uboot loads the kernel from emmc ont the imx8mp

跳至解决方案
1,331 次查看
chen-wust
Contributor II

Currently, we load the kernel from emmc at 31.1m/s. I would like to ask if it is possible to increase this speed by configuring emmc's device tree. What is the maximum loading speed that can be achieved under the condition of sufficient hardware resources

0 项奖励
回复
1 解答
1,313 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

It depends on the eMMC but you can increase the speed by 50 mS.

Regards

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,314 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

It depends on the eMMC but you can increase the speed by 50 mS.

Regards

 

0 项奖励
回复
1,303 次查看
chen-wust
Contributor II

I have changed his bus mode to improve read/write speed, and it does improve read/write speed. However, it will lead to the following problems, making the running speed of other modules slow down a lot.

https://community.nxp.com/t5/i-MX-Processors/Boot-speed-of-the-imx-8plus-Why-is-the-kernel-slow-to-i...


In particular, when using HS400 (read/write rate 70M/S), the uboot boot time is 3s longer, and the kernel boot time is 1s longer.
When using HS200 (read/write rate of 60M/S), although the uboot boot time is 1s less, the kernel boot time is 1s longer.
I think emmc seems to take a long time to initialize when I switch to high speed mode, so the overall boot time doesn't improve. I don't think it's normal that emmc initialization is so slow. In hs200 mode, emmc in the kernel is not initialized properly. In hs400 mode, both the kernel and uboot are slow to initialize emmc. Any good advice on this problem?

 

0 项奖励
回复