uboot for MX8MM can't authenticate kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uboot for MX8MM can't authenticate kernel

Jump to solution
2,918 Views
adam_m
Contributor II

I am working on getting uboot to load a secure kernel on a Boundary Devices Nitrogen8MM. I have already worked through the instructions at https://boundarydevices.com/high-assurance-boot-hab-i-mx8m-edition/ and eveything is working with a sigend uboot.

According to BoundaryDevices, they have been told by NXP that the next step is to get booi to auth the kernel by using this patch: https://github.com/boundarydevices/u-boot-imx6/commit/a20a5ee3c0 However, it's not working.

When I auth the kernel by hand using hab_auth_img, it appears to work just fine:

=> load mmc 1 ${loadaddr} Image
30009696 bytes read in 679 ms (42.1 MiB/s)
=> hab_auth_img ${loadaddr} ${filesize} 0x01c9d000

Authenticate image from DDR location 0x40480000...

Secure boot enabled

HAB Configuration: 0xcc, HAB State: 0x99
No HAB Events Found!

=>


But when just booting I get this:

Authenticating Image...

Authenticate image from DDR location 0x40800000...
Error: Invalid IVT structure

Allowed IVT structure:
IVT HDR = 0x4X2000D1
IVT ENTRY = 0xXXXXXXXX
IVT RSV1 = 0x0
IVT DCD = 0x0
IVT BOOT_DATA = 0xXXXXXXXX
IVT SELF = 0xXXXXXXXX
IVT CSF = 0xXXXXXXXX
IVT RSV2 = 0x0
Authenticate Image Fail, Please check
Error loading kernel image


And, of course, if I don't use the patch then it boots just fine, but I need to auth the kernel before leading.

What am I missing?

0 Kudos
Reply
1 Solution
2,862 Views
adam_m
Contributor II

It turns out the the kernel was being loaded at a non-standard location, so the signing script needed changed.

View solution in original post

2 Replies
2,867 Views
Yuri
NXP Employee
NXP Employee

@adam_m 
Hello,

1.  Please check if parameters "ld", "image_size" in patch function  authenticate_image(ld, image_size)
are the same as in case of manual verification - 

hab_auth_img ${loadaddr} ${filesize}


2. Is IVT added to the kernel before signing?

 

Regards,
Yuri.

0 Kudos
Reply
2,863 Views
adam_m
Contributor II

It turns out the the kernel was being loaded at a non-standard location, so the signing script needed changed.