maybe I am just too old school but I can not for the life of me find the u-boot xxx_defconfig for the iMX8.
I am use to seeing a file like imx6q_logic_defconfig in the uboot-imx/configs folder for the evk boards.
Even the latest "i.MX porting guide" explains it this way.
I need to create a custom uboot for our board that is based off of the iMX8m mini evk.
I cloned the imx_v2018.03_4.14.98_2.0.0_ga uboot-imx.
Maybe I am looking in the wrong place, where should I be looking?
已解决! 转到解答。
I would suggest to read this document instead:
i.MX8 Boot process and creating a bootable image
Hi David
one can look at toradex tutorial:
Build Apalis iMX8/Colibri iMX8X Boot Image/Linux from Scratch
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------