Hi,
Now i'm trying ddr stress test on my board(imx6q) in u-boot,
but i can not set VDD_SOC_CAP/VDD_ARM_CAP 1.325v.(Max is 1.3v)
How can i set more than 1.3v VDD?
below is uboot log:
=====================================
Would do you want to change VDD_SOC_CAP/VDD_ARM_CAP voltage? Type 'y' to run and 'n' to skip
Please select VDD_SOC_CAP volatage on the board
Type 0 for 1.15V; 1 for 1.175V; 2 for 1.2V; 3 for 1.225V; 4 for 1.25V; 5 for 1.275V; 6 for 1.3V