uboot ddr stress tester can not set VDD 1.325v like windows tester

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uboot ddr stress tester can not set VDD 1.325v like windows tester

ソリューションへジャンプ
1,422件の閲覧回数
xiangkunkong
Contributor II

Hi,

Now i'm trying ddr stress test on my board(imx6q) in u-boot,

but i can not set VDD_SOC_CAP/VDD_ARM_CAP 1.325v.(Max is 1.3v)

How can i set more than 1.3v VDD?

 

below is uboot log:

=====================================

Would do you want to change VDD_SOC_CAP/VDD_ARM_CAP voltage? Type 'y' to run and 'n' to skip

Please select VDD_SOC_CAP volatage on the board
Type 0 for 1.15V; 1 for 1.175V; 2 for 1.2V; 3 for 1.225V; 4 for 1.25V; 5 for 1.275V; 6 for 1.3V

 

0 件の賞賛
返信
1 解決策
1,408件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi xiangkunkong

 

one can try to change them using PMU_REG_CORE register described in

sect.50.7.4 Digital Regulator Core Register (PMU_REG_COREn)

i.MX 6Dual/6Quad Applications Processor Reference Manual

 

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,409件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi xiangkunkong

 

one can try to change them using PMU_REG_CORE register described in

sect.50.7.4 Digital Regulator Core Register (PMU_REG_COREn)

i.MX 6Dual/6Quad Applications Processor Reference Manual

 

Best regards
igor

0 件の賞賛
返信
1,398件の閲覧回数
xiangkunkong
Contributor II

Hi igor, 

 

Thanks for your reply. it works for me.

 

Best regards!

Kong

0 件の賞賛
返信