Dear all,
Ii need to build uboot images for i.MX 35 target.But I am facing so many errors to build ltib.
I am using Ubuntu 14.04 64 bit host machine.
Please share steps immediately.
Is it any another way to build images for imx 35.
解決済! 解決策の投稿を見る。
You can git clone U-boot and kernel mainline and build them manually. No need to use LTIB.
For building U-boot mainline for mx35pdk:
export ARCH=arm
export CROSS_COMPILE=/usr/bin/arm-linux-gnueabi-
make mrproper
make mx35pdk_config
make
Regards,
Fabio Estevam
元の投稿で解決策を見る
Dear Sir,
Thanks...
But,I have downloaded L2.6.31_09.12.01 SDK.I want to do flashing using NAND Flash.
So,I need u-boot-3ds.bin.From where I can get uboot,kernel.
Please help me in which matter.I am looking forward to your reply
Thanks
I need link of git for uboot and kernel.
Regards
Hemant
If you want to use FSL U-boot and kernel you can find them at: Freescale Public GIT
If you want to use mainline U-boot: git.denx.de Git
If you want to use mainline kernel: https://www.kernel.org/
I have done with u-boot.
But I need Kernel link(I just found git link for imx 25 but not for imx 35) and its compilation steps like which branch should I choose make..... steps.
Please........
Best Regards
Which U-boot and kernel version do you want to use?
I have downloaded Linux bundle from website,but It is for LTIB.
I need u-boot(for NAND FLASH) and linux 2.6.. version of kernel specially for i.MX35.
In git repository, only imx25 kernel is present.
hemant
Can't you use mainline U-boot and mainline kernel instead?
But I need Kernel link(I just found git link for imx 25 but not for imx 35) and its compilation steps.