Hi
please check that is used correct version of MFG Tools
Programmers (Flash, etc.) (12)
IMX6_M6.0.1_1.0.0_MFG_TOOL (REV M6.0.1_1.0.0)
i.MX 6 Family Manufacturing Toolkit for M6.0.1_1.0.0 (3.14 kernel)
http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...
Then use appropriate *.vbs file for each boot device and processor, for example for i.MX6Q Sabre SD SD card:
mfgtool2-android-mx6q-sabresd-sd.vbs
for eMMC:
mfgtool2-android-mx6q-sabresd-emmc.vbs
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------