Hello, I created on sd card two partition, one EXT4 with root filesytem and secound FAT32 with devicetree and kernel. When I run Your img from ftp-image it's works. But when I try build my own image I got error:
sh: cannot set terminal process group(-1): Inappropriate ioctl for device
sg: no job control in this shell
sh-4.4#
I try run:
su - -c bash
bash: cannot set terminal process group(1): Inappropriate ioctl for device
bash: no job control in this shell
bash-4.4#
my settings are:
setenv mmcroot /dev/mmcblk1p5 rw
setenv bootargs console=${console},${baudrate} ${bootargs_linux} root=${mmcroot} ${bootargs_once} ${extra_bootargs}
setenv load_kernel_mmc fatload mmc 0:6 ${loadaddr} /image.bin
setenv load_fdt_mmc fatload mmc 0:6 ${fdt_addr} /image.dtb
setenv bootcmd 'mmc rescan; run load_kernel_mmc; run load_fdt_mmc; bootz ${loadaddr} - ${fdt_addr}'
saveenv
I have image.bin and image.dtb on sixth partition
If I must make some change in kernel configuration ??
Regards
Adrian
Thanks for answer. But I don't think that is problem with creating image on sd card because when I try use nfs it also don't work.
Regards
Adrian
Ok I removed all my build files and try build image without any package, so now it's work. :smileywink:
Regards
Adrian
Hi Adrian
one can try to follow procedure described in Linux Guide included in
nxp official linux documentation on below link
Use mfg tool from that link for flashing sd image.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------