uSDHCx_VEND_SPEC changing CD_POL bit in uboot or device tree

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uSDHCx_VEND_SPEC changing CD_POL bit in uboot or device tree

ソリューションへジャンプ
1,682件の閲覧回数
deljo_davis
Contributor I

I have a customised Imx6ull board. Imx6ull default uSDHC1 card detect is active low deafult but in our case SD card connector have active high card detect signal. So in my case till uboot only load after that error message will come. I have to make the CD_POL bit at uSDHCx_VEND_SPEC to 1 so that CD will become active high But i dont know where this change need to done. I think changing either in device tree or uboot will work. Anybody know where to change this bit?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,644件の閲覧回数
deljo_davis
Contributor I

Resolved this thing. in device tree under uSDHC1 section CD pin gave as ACTIVE HIGH.

元の投稿で解決策を見る

2 返答(返信)
1,645件の閲覧回数
deljo_davis
Contributor I

Resolved this thing. in device tree under uSDHC1 section CD pin gave as ACTIVE HIGH.

1,644件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Deljo Davis, 

Thank you for sharing your findings. I'm sure they will help other community users.

Regards,

0 件の賞賛
返信