u disk(U盘升级文件系统,内核,uboot)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

u disk(U盘升级文件系统,内核,uboot)

753件の閲覧回数
yuhundehao
Contributor III

I want to use the USB upgrade uboot kernel and file system system how to deal with?

I use this command if=/media/sda/update/uImage of=/dev/mmcblk0 bs=512 seek=2 skip=2 conv=fsync DD can realize the burning of the kernel, then uboot and file system how to operate it

I used the imx6q's board.

ラベル(1)
1 返信

579件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

When the rootfs is running on mmcblk0, you cannot upgrade the new rootfs to mmcblk0. You need to boot the board from other media (such as nand flash, nor flash). Or through USB/serial download mode like MFGtool. Or like Android that has a recovery mode for upgrade used.