u disk(U盘升级文件系统,内核,uboot)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

u disk(U盘升级文件系统,内核,uboot)

864 Views
yuhundehao
Contributor III

I want to use the USB upgrade uboot kernel and file system system how to deal with?

I use this command if=/media/sda/update/uImage of=/dev/mmcblk0 bs=512 seek=2 skip=2 conv=fsync DD can realize the burning of the kernel, then uboot and file system how to operate it

I used the imx6q's board.

Labels (1)
1 Reply

690 Views
jimmychan
NXP TechSupport
NXP TechSupport

When the rootfs is running on mmcblk0, you cannot upgrade the new rootfs to mmcblk0. You need to boot the board from other media (such as nand flash, nor flash). Or through USB/serial download mode like MFGtool. Or like Android that has a recovery mode for upgrade used.