u-boot.nand oob size 64 or 128

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

u-boot.nand oob size 64 or 128

1,184 次查看
IvanRia
Contributor II

I have a system on an mx28evk chip, I have two types of nand memory, one with 64 bytes, the other 128 bytes, I am building a buildroot, I need a universal firmware for both types of memory, I found how to patch uboot so that it works with both memory types, but buildroot has an option for u-boot.nand NAND OOB size, which is not recognized by the bootloader during boot, but is hardcoded in u-boot.nand, 

accordingly, if I set u-boot.nand oob size to 128 bytes, then the system with 64 memory will not boot and vice versa, tell me, is it possible to somehow create a universal firmware for both types of nand memory?

标记 (4)
0 项奖励
回复
1 回复

1,179 次查看
IvanRia
Contributor II

the code in uboot/drivers/mtd/nand/nand_base.c recognizes the OOB size correctly, but mxsboot cant set up OOB size universally, only one OOB size can be passed to the mxsboot, respectively, the question is how you can set the environment variable to uboot from a file uboot/drivers/mtd/nand/nand_base.c?

0 项奖励
回复