u-boot is not booting on imx6 custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

u-boot is not booting on imx6 custom board

1,222 Views
manasa
Contributor I

Hi,

I have an imx6q custom board with two DDR3 chips,size of each DDR3 is 2Gb(32 bit data bus).

I am loading u-boot in serial downloader mode. U-boot is loaded using imx usb loader.It is not giving any error.

After loading u-boot, no messages are printing on tty console(minicom).

Uart1 is used and it is working fine.

I have set new calibration values in cfg file(800mhz_2x128mx16.cfg),those values are

0x021B080C = 0x000F001F

0x021B0810 = 0x0029001C

0x021B083C = 0x0330033C

0x021B0840 = 0x0330032C

0x021B0848 = 0x3E323238

0x021B0850 = 0x383A403E

I have attached cfg file and c file. Anything to be changed in these files for booting of u-boot?

What can be done for booting u-boot?

Thank you

Labels (1)
0 Kudos
Reply
1 Reply

1,113 Views
igorpadykov
NXP Employee
NXP Employee

Hi m20

one can try with nxp uboot

uboot-imx - i.MX U-Boot 

for porting uboot use Porting Guide included in

Linux L4.14.98_2.0.0 Documentation

usb loader is not supported by nxp, one can try steps described in linux

documentation for sd/emmc or nfs boot.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply