u-boot.imx dcd table size

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

u-boot.imx dcd table size

Jump to solution
3,359 Views
xiongweihuang
Contributor III

Hello all

I get the source from http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/log/?h=imx_v2013.04_3.10.17_1.0.0_beta

And after build with several boards config

I notice you get the u-boot.bin from 32k offset in u-boot.imx

Is there any special reason for this ?

With previous version , you start the real u-boot code from 1k offset

How Freescale boot rom support boot from different offset ?

or

Is this a bug ?

Tags (4)
0 Kudos
Reply
1 Solution
2,690 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
6 Replies
2,691 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
2,690 Views
xiongweihuang
Contributor III

Thanks Yixing

Please close this

Regards

0 Kudos
Reply
2,690 Views
YixingKong
Senior Contributor IV

Weihuang

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply
2,690 Views
JasonZhao
Contributor V

Hi, xiongweihuang

Where do you find the 32k offset, As I know, there is 20KB offset in 2013.04, the true u-boot code locate in 0x5000.

0 Kudos
Reply
2,690 Views
YixingKong
Senior Contributor IV

JasonZhao, could you help this customer's question please?

Thanks,

Yixing

0 Kudos
Reply
2,690 Views
Wlodek_D_
Senior Contributor II

Dear xiongweihuang,

Thank you for your post, however please consider moving it to the right community place for better visibility.

For details please see general advice https://community.freescale.com/docs/DOC-99909

Thank you for using Freescale Community.

Regards,

Wlodek_D.

0 Kudos
Reply