u-boot from code aurora fails to build

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

u-boot from code aurora fails to build

3,319件の閲覧回数
andrea_tomasset
Contributor II

Hi,

I know that this exact question has already been asked and, partially, solved here: u-boot from code aurora fails to build 

So, it's even more disappointing that after 6 months I had to re-ask the same question.

Using bitbake to compile u-boot-imx-2018.03 FAILS!!!

The problem is that CONFIG_SYS_CONFIG_NAME is not defined! But defining it as CONFIG_SYS_CONFIG_NAME=mx6sabresd leads to multiple macro redefinition errors.

How am I suppose to fix this?

Here the steps to reproduce the issue:

repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m imx-4.14.98-2.0.0_machinelearning.xml
repo sync
DISTRO="fsl-imx-xwayland" MACHINE="imx6qdlsabresd" source ./fsl-setup-release.sh -b build.xwayland
bitbake u-boot

Error:

/path/to/build.xwayland$ bitbake u-boot
Loading cache: 100% |###############################################################################################################################################################################| Time: 0:00:00
Loaded 3499 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION           = "1.38.0"
BUILD_SYS            = "x86_64-linux"
NATIVELSBSTRING      = "ubuntu-16.04"
TARGET_SYS           = "arm-poky-linux-gnueabi"
MACHINE              = "imx6qdlsabresd"
DISTRO               = "fsl-imx-xwayland"
DISTRO_VERSION       = "4.14-sumo"
TUNE_FEATURES        = "arm armv7a vfp neon callconvention-hard cortexa9"
TARGET_FPU           = "hard"
meta                 
meta-poky            = "HEAD:c9bd4984f8f471ca2c43052714f4413ba99cf171"
meta-oe              
meta-multimedia      = "HEAD:8760facba1bceb299b3613b8955621ddaa3d4c3f"
meta-freescale       = "HEAD:27ca94f8a4336790ba117b4298566f6820e7e74c"
meta-freescale-3rdparty = "HEAD:82037216280a39957fb4272581637abec734ad50"
meta-freescale-distro = "HEAD:f7e2216e93aff14ac32728a13637a48df436b7f4"
meta-bsp             
meta-sdk             = "HEAD:8eeb420fad668b733ab95b460895e1c337c66b25"
meta-browser         = "HEAD:75640e14e325479c076b6272b646be7a239c18aa"
meta-gnome           
meta-networking      
meta-python          
meta-filesystems     = "HEAD:8760facba1bceb299b3613b8955621ddaa3d4c3f"
meta-qt5             = "HEAD:d4e7f73d04e8448d326b6f89908701e304e37d65"
meta-imx-machinelearning = "HEAD:7e9294dead55d1f6b4f1cfe486e0c4e0c5097953"
workspace            = "<unknown>:<unknown>"

Initialising tasks: 100% |##########################################################################################################################################################################| Time: 0:00:00
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: u-boot-imx-2018.03-r0 do_compile: oe_runmake failed
ERROR: u-boot-imx-2018.03-r0 do_compile: Function failed: do_compile (log file is located at /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/temp/log.do_compile.7848)
ERROR: Logfile of failure stored in: /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/temp/log.do_compile.7848
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make -j 8 CROSS_COMPILE=arm-poky-linux-gnueabi- CC=arm-poky-linux-gnueabi-gcc  --sysroot=/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot V=1 HOSTCC=gcc  -isystem/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/include -O2 -pipe -L/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/lib -L/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/lib -Wl,-rpath-link,/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/lib -Wl,-rpath,/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/lib -Wl,-O1 PYTHON=nativepython STAGING_INCDIR=/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/include STAGING_LIBDIR=/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/lib -C /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git O=/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/build mx6sabresd_defconfig
| make: Entering directory '/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git'
| make -C /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/build KBUILD_src=/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git \
| -f /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/Makefile mx6sabresd_defconfig
| make[1]: Entering directory '/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/build'
| make -f /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/scripts/Makefile.build obj=scripts/basic
| ln -fsn /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git source
| /bin/sh /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/scripts/mkmakefile \
|     /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git . 2018 03
|   GEN     ./Makefile
|   gcc  -isystem/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/include -O2 -pipe -L/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/lib -L/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/lib -Wl,-rpath-link,/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/lib -Wl,-rpath,/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/lib -Wl,-O1 -Wp,-MD,scripts/basic/.fixdep.d -Iscripts/basic -Wall -Wstrict-prototypes -O2 -fomit-frame-pointer -o scripts/basic/fixdep /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/scripts/basic/fixdep.c
| rm -f .tmp_quiet_recordmcount
| make -f /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/scripts/Makefile.build obj=scripts/kconfig mx6sabresd_defconfig
|   gcc  -isystem/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/include -O2 -pipe -L/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/lib -L/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/lib -Wl,-rpath-link,/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/lib -Wl,-rpath,/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/lib -Wl,-O1 -Wp,-MD,scripts/kconfig/.zconf.tab.o.d -Iscripts/kconfig -Wall -Wstrict-prototypes -O2 -fomit-frame-pointer -D_GNU_SOURCE -D_DEFAULT_SOURCE -DCURSES_LOC="<ncurses.h>" -DNCURSES_WIDECHAR=1 -DLOCALE  -I/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/scripts/kconfig -Iscripts/kconfig -c -o scripts/kconfig/zconf.tab.o scripts/kconfig/zconf.tab.c
|   gcc  -isystem/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/include -O2 -pipe -L/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/lib -L/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/lib -Wl,-rpath-link,/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/lib -Wl,-rpath,/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/lib -Wl,-O1  -o scripts/kconfig/conf scripts/kconfig/conf.o scripts/kconfig/zconf.tab.o
| scripts/kconfig/conf  --defconfig=arch/../configs/mx6sabresd_defconfig Kconfig
| #
| # configuration written to .config
| #
| make[1]: Leaving directory '/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/build'
| make: Leaving directory '/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git'
| NOTE: make -j 8 CROSS_COMPILE=arm-poky-linux-gnueabi- CC=arm-poky-linux-gnueabi-gcc  --sysroot=/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot V=1 HOSTCC=gcc  -isystem/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/include -O2 -pipe -L/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/lib -L/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/lib -Wl,-rpath-link,/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/lib -Wl,-rpath,/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/lib -Wl,-O1 PYTHON=nativepython STAGING_INCDIR=/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/include STAGING_LIBDIR=/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/lib -C /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git O=/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/build all
| make: Entering directory '/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git'
| make -C /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/build KBUILD_src=/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git \
| -f /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/Makefile all
| make[1]: Entering directory '/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/build'
| make -f /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/Makefile silentoldconfig
| make -f /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/scripts/Makefile.build obj=scripts/basic
| ln -fsn /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git source
| /bin/sh /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/scripts/mkmakefile \
|     /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git . 2018 03
| rm -f .tmp_quiet_recordmcount
|   GEN     ./Makefile
| make -f /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/scripts/Makefile.build obj=scripts/kconfig silentoldconfig
| mkdir -p include/config include/generated
| test -e include/generated/autoksyms.h || \
|     touch   include/generated/autoksyms.h
| scripts/kconfig/conf  --silentoldconfig Kconfig
| make -f /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/scripts/Makefile.autoconf || \
|  { rm -f include/config/auto.conf; false; }
| mkdir -p include/asm
| if [ -d /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/arch/arm/mach-mx6/include/mach ]; then \
|  dest=arch/arm/mach-mx6/include/mach;   \
| else         \
|  dest=arch/arm/include/asm/arch-mx6; \
| fi;         \
| ln -fsn /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/$dest include/asm/arch
| set -e; : '  CHK     include/config.h'; mkdir -p include/;  (echo "/* Automatically generated - do not edit */"; for i in $(echo "IMX_CONFIG=arch/arm/mach-imx/spl_sd.cfg" | sed 's/,/ /g'); do echo \#define CONFIG_$i | sed '/=/ {s/=/ /;q; } ; { s/$/ 1/; }'; done; echo \#define CONFIG_BOARDDIR board/; echo \#include \<config_defaults.h\>; echo \#include \<config_uncmd_spl.h\>; echo \#include \<configs/.h\>; echo \#include \<asm/config.h\>; echo \#include \<linux/kconfig.h\>; echo \#include \<config_fallbacks.h\>;) < /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/scripts/Makefile.autoconf > include/config.h.tmp; if [ -r include/config.h ] && cmp -s include/config.h include/config.h.tmp; then rm -f include/config.h.tmp; else : '  UPD     include/config.h'; mv -f include/config.h.tmp include/config.h; fi
|   arm-poky-linux-gnueabi-gcc  --sysroot=/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot -x c -DDO_DEPS_ONLY -M -MP -Wall -Wstrict-prototypes -Wno-format-security -fno-builtin -ffreestanding -fshort-wchar -Os -fno-stack-protector -fno-delete-null-pointer-checks -g -fstack-usage -Wno-format-nonliteral -Werror=date-time  -D__KERNEL__ -D__UBOOT__   -D__ARM__ -marm -mno-thumb-interwork  -mabi=aapcs-linux  -mword-relocations  -fno-pic  -mno-unaligned-access  -ffunction-sections -fdata-sections -fno-common -ffixed-r9  -msoft-float   -pipe -Iinclude  -I/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/include -I/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/arch/arm/include -include /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/include/linux/kconfig.h  -nostdinc -isystem /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/bin/arm-poky-linux-gnueabi/../../lib/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/7.3.0/include -MQ include/config/auto.conf /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/include/common.h > include/autoconf.mk.dep || { rm include/autoconf.mk.dep; false; }
|   arm-poky-linux-gnueabi-gcc  --sysroot=/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot -E -Wall -Wstrict-prototypes -Wno-format-security -fno-builtin -ffreestanding -fshort-wchar -Os -fno-stack-protector -fno-delete-null-pointer-checks -g -fstack-usage -Wno-format-nonliteral -Werror=date-time  -D__KERNEL__ -D__UBOOT__   -D__ARM__ -marm -mno-thumb-interwork  -mabi=aapcs-linux  -mword-relocations  -fno-pic  -mno-unaligned-access  -ffunction-sections -fdata-sections -fno-common -ffixed-r9  -msoft-float   -pipe -Iinclude  -I/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/include -I/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/arch/arm/include -include /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/include/linux/kconfig.h  -nostdinc -isystem /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/recipe-sysroot-native/usr/bin/arm-poky-linux-gnueabi/../../lib/arm-poky-linux-gnueabi/gcc/arm-poky-linux-gnueabi/7.3.0/include  -DDO_DEPS_ONLY -dM /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/include/common.h > u-boot.cfg.tmp && { grep 'define CONFIG_' u-boot.cfg.tmp > u-boot.cfg; rm u-boot.cfg.tmp; } || { rm u-boot.cfg.tmp; false; }
| In file included from /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/include/common.h:21:0:
| include/config.h:6:10: fatal error: configs/.h: No such file or directory
|  #include <configs/.h>
|           ^~~~~~~~~~~~
| compilation terminated.
| In file included from /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/include/common.h:21:0:
| include/config.h:6:10: fatal error: configs/.h: No such file or directory
|  #include <configs/.h>
|           ^~~~~~~~~~~~
| compilation terminated.
| /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/scripts/Makefile.autoconf:50: recipe for target 'include/autoconf.mk.dep' failed
| make[2]: *** [include/autoconf.mk.dep] Error 1
| make[2]: *** Waiting for unfinished jobs....
| /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git/scripts/Makefile.autoconf:79: recipe for target 'u-boot.cfg' failed
| make[2]: *** [u-boot.cfg] Error 1
| make[1]: *** No rule to make target 'include/config/auto.conf', needed by 'include/config/uboot.release'.  Stop.
| make[1]: Leaving directory '/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/build'
| Makefile:150: recipe for target 'sub-make' failed
| make: *** [sub-make] Error 2
| make: Leaving directory '/path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/git'
| ERROR: oe_runmake failed
| WARNING: /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/temp/run.do_compile.7848:1 exit 1 from 'exit 1'
| ERROR: Function failed: do_compile (log file is located at /path/to/build.xwayland/tmp/work/imx6qdlsabresd-poky-linux-gnueabi/u-boot-imx/2018.03-r0/temp/log.do_compile.7848)
ERROR: Task (/path/to/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/u-boot/u-boot-imx_2018.03.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 829 tasks of which 828 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
  /path/to/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/u-boot/u-boot-imx_2018.03.bb:do_compile
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
ラベル(2)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

3,069件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

This error could be caused by the machine you're trying to use, please see the following, these are the i.MX machine configuration files that can be selected for the i.MX 6:

 

• imx6qpsabreauto

• imx6qpsabresd

• imx6ulevk

• imx6ulz14x14evk

• imx6ull14x14evk

• imx6ull9x9evk

• imx6dlsabreauto

• imx6dlsabresd

• imx6qsabreauto

• imx6qsabresd

• imx6slevk

• imx6solosabreauto

• imx6solosabresd

• imx6sxsabresd

• imx6sxsabreauto

• imx6sllevk

i.e. for the i.MX6Q sabresd

repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m imx-4.14.98-2.0.0_machinelearning.xml
repo sync
DISTRO=fsl-imx-xwayland MACHINE=imx6qsabresd source fsl-setup-release.sh -b build.xwayland
bitbake u-boot

Hope this helps,

Best regards,

Aldo.

0 件の賞賛
返信

3,069件の閲覧回数
andrea_tomasset
Contributor II

Hi nxf46838,

I used the configuration: meta-freescale/conf/machine/imx6qdlsabresd.conf because, if you open it, inside there is a nice comment:

#@TYPE: Machine
#@NAME: NXP i.MX6QP/Q/DL SABRE Smart Device
#@SOC: i.MX6QP/Q/DL
#@DESCRIPTION: Machine configuration for NXP i.MX6QP/Q/DL SABRE Smart Device
#@MAINTAINER: Otavio Salvador <otavio@ossystems.com.br>
#
# This machine replaces the following machines:
#    * imx6qpsabresd
#    * imx6qsabresd
#    * imx6dlsabresd
#    * imx6solosabresd
# and is able to work for all the machines.

So, I understood that that configuration should be meant to replace also the machine that I was needing: imx6qsabresd

If it's not the case, the comment is very misleading.

By the way, thank you at least to take the time to reply.

Andrea

0 件の賞賛
返信

3,069件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

As referenced on the i.MX Yocto Project User's Guide, section 5.1 Build configuration:

In the meta-fsl-bsp-release layer, i.MX provides new or updated machine configurations that overlay the meta-freescale machine configurations. These files are copied into the meta-freescale/conf/machine directory by the fsl-setup-release.sh script

If you want to use uboot for an specific target please use one of the mentioned before machines, i.e. imx6qsabresd. Also if need for a common images for the i.MX 6:

In the meta-fsl-bsp-release layer, consolidated machine configurations (imx6qpdlsolox.conf and imx6ul7d.conf) are provided for i.MX 6 and i.MX 7 machines. i.MX uses these to build a common image with all the device trees in one image for testing. Do not use these machines for anything other than testing.

Hope this helps,

Best regards,

Aldo.

0 件の賞賛
返信