u-boot config file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,989件の閲覧回数
goto11
Contributor III

Hello,Community


The following two configuration files are stored in "... / board / freescale / mx7dsabresd".
What is the difference between the files?
How should I use files properly?


imximage.cfg
imximage_TO_1_1.cfg

best regards

Goto

ラベル(1)
1 解決策
1,897件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

it seems the silicon version, imximage_TO_1_1.cfg should be the latest version, for detailed information, you can refer to your own i.mx7d DCD settings, I compare these two files, imximage_TO_1_1.cfg add DDR_PHY settings and Anadig DDR PLL Control Register

元の投稿で解決策を見る

1 返信
1,898件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

it seems the silicon version, imximage_TO_1_1.cfg should be the latest version, for detailed information, you can refer to your own i.mx7d DCD settings, I compare these two files, imximage_TO_1_1.cfg add DDR_PHY settings and Anadig DDR PLL Control Register