u-boot config file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

u-boot config file

Jump to solution
1,002 Views
goto11
Contributor III

Hello,Community


The following two configuration files are stored in "... / board / freescale / mx7dsabresd".
What is the difference between the files?
How should I use files properly?


imximage.cfg
imximage_TO_1_1.cfg

best regards

Goto

Labels (1)
1 Solution
910 Views
joanxie
NXP TechSupport
NXP TechSupport

it seems the silicon version, imximage_TO_1_1.cfg should be the latest version, for detailed information, you can refer to your own i.mx7d DCD settings, I compare these two files, imximage_TO_1_1.cfg add DDR_PHY settings and Anadig DDR PLL Control Register

View solution in original post

1 Reply
911 Views
joanxie
NXP TechSupport
NXP TechSupport

it seems the silicon version, imximage_TO_1_1.cfg should be the latest version, for detailed information, you can refer to your own i.mx7d DCD settings, I compare these two files, imximage_TO_1_1.cfg add DDR_PHY settings and Anadig DDR PLL Control Register