u-boot can't boot from eMMc4.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

u-boot can't boot from eMMc4.4

2,638 Views
zhuhaigang
Contributor I

I buy the Freescale i.MX53 Quick Start board. it's mx53_loco.

I download i.MX53-QSB-Android-Gingerbread-Release4.3 from Reference BSPs for Freescale i.MX53 Quick Start Board.

copy all file of prebulid floder to ..\Profiles\MX53 Linux Update\OS Firmware\files\android\.(Mfgtools tools)

Then open Mfgtools tools,select mx53_smd_android_emmc4.4.   Start ,operation Success.

u-boot can't boot from emmc4.4.

I suspect \Profiles\MX53 Linux Update\OS Firmware\files\ucl.xml is error.so I see it.

ucl.xml :

Please use slot3 for MMC4.4 update

      The following are the valid inputs when configure the boot

      partitions of the eMMC cards.

      +------------------------------------------------------------+

      | Bit7 | Bit6     | Bit5 Bit4 Bit3        | Bit2 Bit1 Bit0   |

      |------|----------|-----------------------|------------------|

      | X    | BOOT_ACK | BOOT_PARTITION_ENABLE | PARTITION_ACCESS |

      +------------------------------------------------------------+

      Bit7: Reserved

      Bit6: always set to vaule '1' when boot_part is enabled

      Bit[5:3]:

      0x0 : Device not boot enabled (default)

      0x1 : Boot partition 1 enabled for boot

      0x2 : Boot partition 2 enabled for boot

      0x7 : User area enabled for boot

      Bit[2:0]:

      0x0 : No access to boot partition (default)

      0x1 : R/W boot partition 1

      0x2 : R/W boot partition 2

      So only the '0, 1, 2; 8, 9, 10; 16, 17, 18; 56, 57, 58' are

      valid parameters when configure the boot_partiton.

<CMD type="push" body="$ echo 1 > /sys/devices/platform/mxsdhci.2/mmc_host/mmc2/mmc2:0001/boot_config">access boot partition 1</CMD>

<CMD type="push" body="$ echo 8 > /sys/devices/platform/mxsdhci.2/mmc_host/mmc2/mmc2:0001/boot_config">access user partition,and enable boot partion1 to boot</CMD>

<CMD type="push" body="$ echo 2 > /sys/devices/platform/mxsdhci.2/mmc_host/mmc2/mmc2:0001/boot_bus_config">Set boot width is 8bits</CMD>


Red color of the sentences I do not know what that means?

by the way,I test successful u-boot boot from eMMc4.4 by the same u-boot.bin,but not use Mfgtools.Steps are as follows

eMMC 4.3 and 4.4 card support fastboot. To boot from fastboot, please follow below steps:

1. Make sure the slot can support fastboot.

Please check spec for this information. On most of our boards, Slot3 support eMMC fastboot.

2. Program u-boot image to eMMC boot partition.

Normal boot from SD first and program u-boot image to boot partition.

e.g

• Insert normal SD card to slot1 and eMMC 4.3/4.4 card to slot3.

• Normal boot from SD slot1.

• Write u-boot.bin to eMMC card boot partition.

e.g

> mmc read 0 ${loadaddr} 0 0x200

MMC read: dev # 0, block # 0,count 512 ...

512 blocks read: OK

> mmc write 1 ${loadaddr} 0 0x200 1

MMC read: dev # 1, block # 0,count 512 ... partition 1

512 blocks write: OK

3. Get eMMC bus width.

Get boot bit bus mode. Use command “mmcinfo <dev>“ to get bus width.

> mmcinfo 1

Device: FSL_ESDHC

Manufacturer ID: 3

OEM: 5344

Name: SD04G

Tran Speed: 25000000

Rd Block Len: 512

SD version 2.0

High Capacity: Yes

Capacity: 3965190144

Bus Width: 4-bit

4. Set eMMC fast boot dip and boot bits.

• Set eMMC fast boot dip.

• Set bus width to the bus width we got from step 3.

5. Reset board for booting.

why u-boot can't boot from eMMc4.4 by Mfgtools?I just say ..


can anybody help me?

Labels (2)
0 Kudos
Reply
1 Reply

1,071 Views
Yuri
NXP Employee
NXP Employee

Strictly speaking the i.MX53 QSB is not equipped with eMMC.

The i.MX53 SMD supports eMMC.

SABRE Platform for Tablets based on i.MX53 Product Summary Page

0 Kudos
Reply