u-boot args with hdmi

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

u-boot args with hdmi

ソリューションへジャンプ
3,535件の閲覧回数
jiejia
Contributor III

while  bootargs=console=ttymxc0,115200 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32,    the egl/gles display well.

while bootargs=console=ttymxc0,115200 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24,bpp=24,    the egl/gles display error.

Why can't I set the bpp=24 while if=RGB24?

ラベル(1)
0 件の賞賛
返信
1 解決策
3,270件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jie

please refer to attached MX_6_Graphics_User's_Guide

sect.6.1.2 24 bpp pixmap :

The GPU can only accelerate a 16 bpp or 32 bpp pixmap.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,271件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi jie

please refer to attached MX_6_Graphics_User's_Guide

sect.6.1.2 24 bpp pixmap :

The GPU can only accelerate a 16 bpp or 32 bpp pixmap.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信