u-boot Splash screen for RGB LCD on i.MX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

u-boot Splash screen for RGB LCD on i.MX6DL

1,310 Views
prasannakulkarni
Contributor IV

Hi,

      How to bring-up splash screen over RGB LCD on i.MXDL platform. by default source has support for only LVDS display splash screen.  I have found a link https://community.nxp.com/thread/335772  which is a similar implementation but it is for i.MXSL EVK, I have tried to adopt the same but didn't work. There is a conflict in ipuv3 and this patch. If this patch is forcibly called then ipuv3 goes for a task and no Android screen comes up further no display at all.  update me if anyone have solved this issue.  

Labels (4)
0 Kudos
Reply
1 Reply

1,198 Views
igorpadykov
NXP Employee
NXP Employee

Hi Prasanna

boundary devices i.mx6 boards have parallel lcds and one can check its resources:

https://boundarydevices.com/displaying-a-splash-screen-with-u-boot/ 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply