u-boot-2017后编译的u-boot.imx无法启动

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

u-boot-2017后编译的u-boot.imx无法启动

938 Views
0609ccj
Contributor I

之前有u-boot-2015 通过以下命令

make ARCH=arm mx6qsabresd_defconfig 

make ARCH=arm u-boot.imx

将编译出来的u-boot.imx放到mfgtool的file文件下,下载到imx6q的emmc中可以正常启动

后面更新了u-boot-2017后,configs里面已经没有mx6qsabresd_defconfig,只有mx6sabresd_defconfig文件

然后编译的u-boot.imx下载到emmc中无法启动,新版本的u-boot修改了那些东西,为什么无法启动了?

Labels (1)
Tags (1)
0 Kudos
2 Replies

817 Views
shivanipatel
Senior Contributor II

Hi changjing chi,

From which link you are downloading the U-Boot version 2017 source?

Please download the u-boot source from this link. In this source, the config "mx6qsabresd_defconfig" is there. I have complied this source and flashed u-boot image on the board. The uboot runs successfully on the board.

Let us know in case of  any concern.

Regards,

Shivani

0 Kudos

817 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Or you can continues using the uboot 2015 if it work for you.

0 Kudos