Hi guys , ihave a mx6q_sabresd but , when i try to run Ltib and compile my Bsp , u-boot crashes !! ... in /board/frescale/mx6q_sabresd no exist !! :smileyplain:
what is the problem..? i need some patches? or a last version of ltib.
Processing: u-boot-v2009.08
=============================
Build path taken because: directory build, no prebuilt rpm,
scbuild/scdeploy already unpacked packageProcessing: u-boot-v2009.08
=============================
Build path taken because: directory build, build key set, no prebuilt rpm,rpmbuild --dbpath /home/imx6/ltib/rootfs//var/lib/rpm --target arm --define '_unpackaged_files_terminate_build 0' --define '_target_cpu arm' --define '__strip strip' --define '_topdir /home/imx6/ltib/rpm' --define '_prefix /usr' --define '_tmppath /home/imx6/ltib/tmp' --define '_rpmdir /home/imx6/ltib/rpm/RPMS' --define '_mandir /usr/share/man' --define '_sysconfdir /etc' --define '_localstatedir /var' -bc --short-circuit /home/imx6/ltib/tmp/u-boot-v2009.08.spec
Building target platforms: arm
Building for target arm
Executing(%build): /bin/sh -e /home/imx6/ltib/tmp/rpm-tmp.58197
+ umask 022
+ cd /home/imx6/ltib/rpm/BUILD
+ cd u-boot-2009.08
+ : mx6q_sabresd_config
+ eval echo
+ echo
+ PKG_U_BOOT_PATH_PRECONFIG=
+ SRC_DIR=/home/imx6/ltib/rpm/BUILD/u-boot-2009.08
+ BUILD_DIR=/home/imx6/ltib/rpm/BUILD/u-boot-2009.08
+ [ /home/imx6/ltib/rpm/BUILD/u-boot-2009.08 != /home/imx6/ltib/rpm/BUILD/u-boot-2009.08 ]
+ cd /home/imx6/ltib/rpm/BUILD/u-boot-2009.08
+ [ -n ]
+ make HOSTCC=ccache /usr/bin/gcc -B/usr/bin/ CROSS_COMPILE=arm-none-linux-gnueabi- O=/home/imx6/ltib/rpm/BUILD/u-boot-2009.08 mx6q_sabresd_config
make: *** No rule to make target `mx6q_sabresd_config'. Stop.
error: Bad exit status from /home/imx6/ltib/tmp/rpm-tmp.58197 (%build)
RPM build errors:
Bad exit status from /home/imx6/ltib/tmp/rpm-tmp.58197 (%build)
Build time for u-boot-v2009.08: 0 seconds
I have the sabresd board and following the EXACT instructions from Freescale's documentation, I was able to boot the system just fine. Do you have the documentation for your board? I think you might need to register to get access to them. It's there on the iMX6Q website.
On a different tangent, I was having trouble getting the latest (2013 version) of u-boot running on the sabresd board and Youngcai (from Freescale) was very helpful in assisting me. You can see the thread here,
https://community.freescale.com/message/342003#342003
Please note: following those instructions will only get u-boot up and running. I wasn't able to figure out how to setup the boot arguments to get the linux kernel (or android) booting off the eMMC after that.
Also; my host is an ubuntu 12.04 64-bit system. I have no idea how to work on fedora or with RPMs.
-Abraham V.