tvp5158 interleaved mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

tvp5158 interleaved mode

跳至解决方案
1,645 次查看
Selea
Senior Contributor I

Ww would like to acquire 4 video channel (pal or ntsc) using TVP5158 in pixel or line interleaved mode so we can have all 4 channels time sharing the same parallel video port (8 or 16 bit).

is it possible to acquire it using the parallel CSI of imx6Q? I mean the CSi can handle such kind of interleaving? and produce 4 different virtual channels (as the mipi seeem to do)??

any suggestion or  question?

Thanks

Omar

标签 (1)
0 项奖励
回复
1 解答
1,246 次查看
jack_mao
NXP Employee
NXP Employee

Hi,

      The CSI  support inteleave mode, we have tired to connect two camera with one CSI before,  but IPU has two CSI, should meet your requiement, you could refer to the reference manual about the detail.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,247 次查看
jack_mao
NXP Employee
NXP Employee

Hi,

      The CSI  support inteleave mode, we have tired to connect two camera with one CSI before,  but IPU has two CSI, should meet your requiement, you could refer to the reference manual about the detail.

0 项奖励
回复