tvp5158 interleaved mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

tvp5158 interleaved mode

Jump to solution
1,000 Views
Selea
Senior Contributor I

Ww would like to acquire 4 video channel (pal or ntsc) using TVP5158 in pixel or line interleaved mode so we can have all 4 channels time sharing the same parallel video port (8 or 16 bit).

is it possible to acquire it using the parallel CSI of imx6Q? I mean the CSi can handle such kind of interleaving? and produce 4 different virtual channels (as the mipi seeem to do)??

any suggestion or  question?

Thanks

Omar

Labels (1)
0 Kudos
1 Solution
601 Views
jack_mao
NXP Employee
NXP Employee

Hi,

      The CSI  support inteleave mode, we have tired to connect two camera with one CSI before,  but IPU has two CSI, should meet your requiement, you could refer to the reference manual about the detail.

View solution in original post

0 Kudos
1 Reply
602 Views
jack_mao
NXP Employee
NXP Employee

Hi,

      The CSI  support inteleave mode, we have tired to connect two camera with one CSI before,  but IPU has two CSI, should meet your requiement, you could refer to the reference manual about the detail.

0 Kudos