tvin display is not clear and its hazy.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

tvin display is not clear and its hazy.

1,500 Views
rajucm
Contributor III

Dear all,

Interface: CSI0-8bit (CSI0_DAT12:CSI0_DAT19), BT656 NTSC std video format without HS and VS.

Now, My TVin driver for video codec TW8836 is up and running.  But, Video quality is not good. Its hazy and we can see line gaps when we wave the hand in front of camera. At bellow Image we can observe.

1) Lines while waving hand

2) 1.5m written in green color is also not very clear.

Is this De-interlacing problem? How to fix? Please suggest me.

Capture.jpg

Thanks,

Rajucm

0 Kudos
Reply
2 Replies

1,310 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Raju,

    Yes, the issue should be de-interlacing problem !  you can use VDIC in CSI to do hardware de-interlace !

    please refter to this paste, it should help you resolve it !

https://community.freescale.com/message/370083#370083

   Hope my advice can help you !

Regards,

Weidong

0 Kudos
Reply

1,310 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Raju,

      if you have resolved your question, please help me correct "Correct button" "Helpful button" to close this ticket !

Thanks!

Regards,

Weidong

0 Kudos
Reply