turn ON of i.MX6 processor from shutdown condition with out using ONOFF

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

turn ON of i.MX6 processor from shutdown condition with out using ONOFF

804 次查看
sadatanvashisth
Contributor II

Also how can I trigger turn ON of processor from shutdown condition with out using ONOFF switch?

0 项奖励
回复
1 回复

764 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   If OFF state means all power supply voltages of the i.MX 6ULL, except VDD_SNVS_IN, are OFF, than

it is impossible to assert any signals (except ONOFF) of the i.MX 6ULL in order to activate an external (PMIC)

power supply scheme.

  If i.MX 6ULL is completely de-energized, then its PMIC_ON_REQ will be asserted automatically

when VDD_SNVS_IN is applied. This allows to switch on all the rest voltages for i.MX 6ULL

from a PMIC.

 


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复