ttymxc1 (uart) not receiving datas

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ttymxc1 (uart) not receiving datas

1,251 次查看
giritharanr
Contributor I


Hi i am new to this,

                                 I have two custom imx6DL boards.But only one difference between two boards(i.e board A is configured with SD1 and board B is configured with SD3).

So in uboot i changed for board B SD1 to SD3 and inmachine driver itself i changed to SD3.

Both boards are configured with same UART pins.(

MX6Q_PAD_SD3_DAT4__GPIO_7_1,

MX6Q_PAD_SD3_DAT5__UART2_TXD,)

My problem is Board A receive datas from microcontroller properly through UART.

But Board B is not at all receiving datas through UART from microcontroller.

I probe the receiver pin.But its toggle.

So whats the issue?how can i solve?

please help me to identify the issue..

With regards,

R.Giritharan

标签 (1)
标记 (3)
0 项奖励
回复
2 回复数

1,002 次查看
art
NXP Employee
NXP Employee

Why do you configure the SD3_DAT4 pin for GPIO function? To make it work as UART RX pin, you have to configure it as UART2_RXD.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,002 次查看
giritharanr
Contributor I

Anybody is there???

0 项奖励
回复