Hi,
I am working with IMX8M Mini EVK and yocto project build details:
Build Configuration:
BB_VERSION = "1.38.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-16.04"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8mmevk"
DISTRO = "fsl-imx-xwayland"
DISTRO_VERSION = "4.14-sumo"
TUNE_FEATURES = "aarch64"
TARGET_FPU = ""
I am able to build the images.
I would like to know the toolchain name and location path.
From the doc: i.MX_Yocto_Project_User's_Guide.pdf
section 5.3 : Building an Image
The Yocto Project build uses the bitbake command. For example, bitbake <component> builds the named component.
Each component build has multiple tasks, such as fetching, configuration, compilation, packaging, and deploying to the target
rootfs. The bitbake image build gathers all the components required by the image and build in order of the dependency per
task. The first build is the toolchain along with the tools required for the components to build.
The following command is an example on how to build an image:
$ bitbake fsl-image-validation-imx
Could you please tell me the toolchain name and location path:
Thank you,
Sreedhar
Solved! Go to Solution.
Hi Sreedhar,
See below, please!
| aarch64-poky-linux-gcc |
|---|
| weidong@ubuntu:~/imx-release-bsp-l4.19.35/build-xwayland-imx8/tmp/work/x86_64-linux/gcc-cross-aarch64/8.3.0-r0/sysroot-destdir/home/weidong/imx-release-bsp-l4.19.35/build-xwayland-imx8/tmp/work/x86_64-linux/gcc-cross-aarch64/8.3.0-r0/recipe-sysroot-native/usr/libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/8.3.0$ ls aarch64-poky-linux-ar aarch64-poky-linux-ld.bfd aarch64-poky-linux-ranlib cc1plus ld libcc1plugin.so.0.0.0 libcp1plugin.so.0 lto1 plugin aarch64-poky-linux-as aarch64-poky-linux-ld.gold aarch64-poky-linux-strip collect2 ld.bfd libcc1.so libcp1plugin.so.0.0.0 lto-wrapper ranlib aarch64-poky-linux-cpp aarch64-poky-linux-nm ar cpp ld.gold libcc1.so.0 liblto_plugin.so nm strip aarch64-poky-linux-gcc aarch64-poky-linux-objcopy as gcc libcc1plugin.so libcc1.so.0.0.0 liblto_plugin.so.0 objcopy aarch64-poky-linux-ld aarch64-poky-linux-objdump cc1 install-tools libcc1plugin.so.0 libcp1plugin.so liblto_plugin.so.0.0.0 objdump weidong@ubuntu:~/imx-release-bsp-l4.19.35/build-xwayland-imx8/tmp/work/x86_64-linux/gcc-cross-aarch64/8.3.0-r0/sysroot-destdir/home/weidong/imx-release-bsp-l4.19.35/build-xwayland-imx8/tmp/work/x86_64-linux/gcc-cross-aarch64/8.3.0-r0/recipe-sysroot-native/usr/libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/8.3.0$ |
Have a nice day!
B.R,
Weidong
Hello Sreedhar,
In i.MX_Linux_User's_Guide.pdf, it is described on how to operate standalone mode and how to export tool chain.
you can do like this:
--->compiling image
1. DISTRO=fsl-imx-xwayland MACHINE=imx8mmevk source fsl-setup-release.sh -b build-xwayland
2. bitbake core-image-minimal
--->exporting tool chain
1.Using the command to export toolchain SDK.
#DISTRO=fsl-imx-xwayland MACHINE=imx8mmevk bitbake core-image-minimal -c populate_sdk
Then you will get a .sh file including tool chain, see below, please!
2. Copy the file to /opt/
# cd ~/imx-yocto-bsp/build-xwayland/tmp/deploy/sdk
# sudo cp ./fsl-imx-xwayland-glibc-x86_64-core-image-minimal-aarch64-toolchain-4.14-sumo.sh /opt
# cd /opt
# sudo ././fsl-imx-xwayland-glibc-x86_64-core-image-minimal-aarch64-toolchain-4.14-sumo.sh
Then according to guidance to install toolchain to /opt directory or other director you like.
Below is mine:
3. Before starting to opreate standalone, environment must be set.
Below is linux and u-boot source code on my ubuntu:
Set environment:
# source /opt/Cortex-A53-L4.14.98-2.0.0-toolchain/4.14-sumo/environment-setup-aarch64-poky-linux
The command indicates the CROSS_COMPILE environment has been ready.
Now you can use "make" to compile u-boot or linux source code.
Hope above contents are helpful to you!
Have a nice day!
B.R,
Weidong
Hi Weidong,
Thank you for the details!!
From the doc: i.MX_Yocto_Project_User's_Guide.pdf section 5.3
"The first build is the toolchain along with the tools required for the components to build"
without exporting the toolchain we can build the entire distribution
We build the distribution as below:
1. DISTRO=fsl-imx-xwayland MACHINE=imx8mmevk source fsl-setup-release.sh -b build-xwayland
2. bitbake fsl-image-validation-imx
sdcard images are created in the deploy directory : /deploy/images/imx8mmevk/
by exporting the toolchain as mentioned in the details by you, we can know the toolchain name and path.
If we don't export the toolchain, can we know the toolchain name and path used for building the distribution?
Can you tell me the toolchain path and name without exporting.
Regards,
Sreedhar
Hi Sreedhar,
See below, please!
| aarch64-poky-linux-gcc |
|---|
| weidong@ubuntu:~/imx-release-bsp-l4.19.35/build-xwayland-imx8/tmp/work/x86_64-linux/gcc-cross-aarch64/8.3.0-r0/sysroot-destdir/home/weidong/imx-release-bsp-l4.19.35/build-xwayland-imx8/tmp/work/x86_64-linux/gcc-cross-aarch64/8.3.0-r0/recipe-sysroot-native/usr/libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/8.3.0$ ls aarch64-poky-linux-ar aarch64-poky-linux-ld.bfd aarch64-poky-linux-ranlib cc1plus ld libcc1plugin.so.0.0.0 libcp1plugin.so.0 lto1 plugin aarch64-poky-linux-as aarch64-poky-linux-ld.gold aarch64-poky-linux-strip collect2 ld.bfd libcc1.so libcp1plugin.so.0.0.0 lto-wrapper ranlib aarch64-poky-linux-cpp aarch64-poky-linux-nm ar cpp ld.gold libcc1.so.0 liblto_plugin.so nm strip aarch64-poky-linux-gcc aarch64-poky-linux-objcopy as gcc libcc1plugin.so libcc1.so.0.0.0 liblto_plugin.so.0 objcopy aarch64-poky-linux-ld aarch64-poky-linux-objdump cc1 install-tools libcc1plugin.so.0 libcp1plugin.so liblto_plugin.so.0.0.0 objdump weidong@ubuntu:~/imx-release-bsp-l4.19.35/build-xwayland-imx8/tmp/work/x86_64-linux/gcc-cross-aarch64/8.3.0-r0/sysroot-destdir/home/weidong/imx-release-bsp-l4.19.35/build-xwayland-imx8/tmp/work/x86_64-linux/gcc-cross-aarch64/8.3.0-r0/recipe-sysroot-native/usr/libexec/aarch64-poky-linux/gcc/aarch64-poky-linux/8.3.0$ |
Have a nice day!
B.R,
Weidong
Thank you Weidong. I got the required answer.