tlv320aic3104 under linux version 4.14,imx8m

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

tlv320aic3104 under linux version 4.14,imx8m

1,006件の閲覧回数
yvonne_chen
Contributor I

Hello Team

 Could anyone tell me is there a working driver for tlv320aic3104 under linux version 4.14 , based on imx8m?

To make tlv320aic3104 works, what driver's components at least that I should port in?

I just found one codec driver named tlv320aic3x.c, where could I get the machine part ?

And is there any thing else I should port and compile? How about the imx sdma?Do I need it to make tlv320aic3104 working?

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

923件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi yvonne

tlv320aic3104 codec is not supported in nxp linux bsps, supported are described

in linux documentation on i.MX Software | NXP 

One can try to port it using example on

https://community.nxp.com/thread/504807 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信