./tlib fails to build kernel-3.0.35

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

./tlib fails to build kernel-3.0.35

2,799 次查看
djbuijs
Contributor I

I am trying to build a kernel for the SABRE iMX6 Quad board and am running into some issues. This is the first time I build a kernel and I am following the provided guide "SABRE_SD_User_Guide_L3.0.35_1.1.0.pdf". The selected kernel version is the default "kernel-3.0.35".

My host is Ubuntu 9.04 (on VirtualBox on Win 7 Pro). I managed to build LTIB without issues.

However, when I start building the kernel (./ltib) I get several errors:

1) ############

     net/core/pktgen.c: In function 'pktgen_if_show':

     net/core/pktgen.c:682:2775: error: can't find a register in class 'GENERAL_REGS' while reloading 'asm'

     net/core/pktgen.c:682:3153: error: can't find a register in class 'GENERAL_REGS' while reloading 'asm'

     net/core/pktgen.c:682:2775: error: 'asm' operand has impossible constraints

     net/core/pktgen.c:682:3153: error: 'asm' operand has impossible constraints

     make[2]: *** [net/core/pktgen.o] Error 1

Line 682 in the file pktgen.c states....I have not gone further than that:

     do_div(idle, NSEC_PER_USEC);

2) ############

     CC [M] net/dccp/ipv4.o

     drivers/scsi/advansys.c:72:2: warning: #warning this driver is still not properly converted to the DMA API [-Wcpp]

     drivers/scsi/advansys.c: In function 'advansys_get_sense_buffer_dma':

     drivers/scsi/advansys.c:8376:2: error: implicit declaration of function 'dma_cache_sync' [-Werror=implicit-function-declaration]

     cc1: some warnings being treated as errors

     make[2]: *** [drivers/scsi/advansys.o] Error 1

     make[1]: *** [drivers/scsi] Error 2

     make[1]: *** Waiting for unfinished jobs....

Additionally this message showed up at the beginning of the build:

     Warning: cannot find a config file for the kernel

This while I did execute the kernel config..... could this be the issue? The script seems to be looking for the file : imx6_defconfig which does not exist.... These are the *defconfig I found:

dirk@dirk-desktop:~/projects/dcns/sabre/src/ltib$

ls ~/projects/dcns/sabre/src/ltib/rpm/BUILD/linux-3.0.35/arch/arm/configs/ | grep mx

mx1_defconfig

mx21_defconfig

mx27_defconfig

mx3_defconfig

mx51_defconfig

mxs_defconfig

As instructed I entered platform type: "imx6q" and "min profile" (the default). I am trying various things now (build different kernel versions, ), but haven't gotten any success yet....

Here's a link to someone who had a similar issue, but it never seems to have gotten resolved...

Help: LTIB build failed

What can be the issue?

Dirk

  

dirk@dirk-desktop:~/projects/dcns/sabre/src/ltib$

######################

Processing: fake-provides

===========================

Processing: u-boot

====================

Processing: kernel-3.0.35

===========================

Build path taken because: build key set, no prebuilt rpm,

rpmbuild --dbpath /home/dirk/projects/dcns/sabre/src/ltib/rootfs//var/lib/rpm --target arm --define '_unpackaged_files_terminate_build 0' --define '_target_cpu arm' --define '__strip strip' --define '_topdir /home/dirk/projects/dcns/sabre/src/ltib/rpm' --define '_prefix /usr' --define '_tmppath /home/dirk/projects/dcns/sabre/src/ltib/tmp' --define '_rpmdir /home/dirk/projects/dcns/sabre/src/ltib/rpm/RPMS'  --define '_mandir /usr/share/man' --define '_sysconfdir /etc' --define '_localstatedir /var' -bb /home/dirk/projects/dcns/sabre/src/ltib/tmp/kernel-3.0.35.spec

Building target platforms: arm

Building for target arm

Executing(%prep): /bin/sh -e /home/dirk/projects/dcns/sabre/src/ltib/tmp/rpm-tmp.41639

+ umask 022

+ cd /home/dirk/projects/dcns/sabre/src/ltib/rpm/BUILD

+ echo imx_1.1.0

+ cut -d_ -f2

+ rel_ver=1.1.0

+ echo imx_1.1.0

+ cut -d. -f3

+ cut -c2

+ zz=

+ git_tag=rel_imx_3.0.35_1.1.0

+ [  != 0 ]

+ git_br=imx_3.0.35_1.1.0

+ KSRC_DIR=/home/dirk/projects/dcns/sabre/src/ltib/rpm/BUILD/linux-3.0.35

+ [ -z y ]

+ [ ! -d /home/dirk/projects/dcns/sabre/src/ltib/rpm/BUILD/linux-3.0.35 ]

+ exit 0

Executing(%build): /bin/sh -e /home/dirk/projects/dcns/sabre/src/ltib/tmp/rpm-tmp.41639

+ umask 022

+ cd /home/dirk/projects/dcns/sabre/src/ltib/rpm/BUILD

+ cd linux-3.0.35

+ eval echo

+ echo

+ PKG_KERNEL_PATH_PRECONFIG=

+ eval echo

+ echo

+ PKG_KERNEL_KBUILD_PRECONFIG=

+ eval echo imx6_defconfig

+ echo imx6_defconfig

+ PKG_KERNEL_PRECONFIG=imx6_defconfig

+ KSRC_DIR=/home/dirk/projects/dcns/sabre/src/ltib/rpm/BUILD/linux-3.0.35

+ : arm

+ : ccache /usr/bin/gcc -B/usr/bin/

+ : imx6_defconfig

+ : /home/dirk/projects/dcns/sabre/src/ltib/config/platform/imx

+ : /home/dirk/projects/dcns/sabre/src/ltib/rpm/BUILD/linux-3.0.35

+ rm -f /home/dirk/projects/dcns/sabre/src/ltib/rpm/BUILD/linux

+ ln -s /home/dirk/projects/dcns/sabre/src/ltib/rpm/BUILD/linux-3.0.35 /home/dirk/projects/dcns/sabre/src/ltib/rpm/BUILD/linux

+ cd /home/dirk/projects/dcns/sabre/src/ltib/rpm/BUILD/linux-3.0.35

+ KBOUT=

+ [ -n  -a  != . ]

+ KBOUT=.

+ KTARG=zImage

+ SYSCFG_KTARG=uImage

+ [ imx6_defconfig = defconfig ]

+ [ -f /home/dirk/projects/dcns/sabre/src/ltib/config/platform/imx/imx6_defconfig.dev ]

+ [ -f /home/dirk/projects/dcns/sabre/src/ltib/config/platform/imx/imx6_defconfig ]

+ [ -z  ]

+ [ -d arch/arm/configs/ ]

+ find arch/arm/configs/ -name imx6_defconfig

+ CFG=

+ [ -n  ]

+ [ -d arch/arm/configs/ ]

+ find arch/arm/configs/ -name imx6_defconfig

+ CFG=

+ [ -n  ]

+ [ arm = ppc -a -f arch/powerpc/Kconfig ]

+ [ -n  ]

+ [ -n  ]

+ echo Warning: cannot find a config file for the kernel

Warning: cannot find a config file for the kernel

+ [ -z  -a -n y -o -n  ]

+ make ARCH=arm CROSS_COMPILE= HOSTCC=ccache /usr/bin/gcc -B/usr/bin/ menuconfig

scripts/kconfig/mconf Kconfig

*** End of the configuration.

*** Execute 'make' to start the build or try 'make help'.

+ [ -f  ]

+ [ -n  ]

+ grep -q VERSION = 2 Makefile

+ [ %{kernel_series} = 2.4 ]

+ make ARCH=arm CROSS_COMPILE= HOSTCC=ccache /usr/bin/gcc -B/usr/bin/ uImage

  CHK include/linux/version.h

  CHK include/generated/utsrelease.h

make[1]: `include/generated/mach-types.h' is up to date.

  CALL scripts/checksyscalls.sh

  CHK     include/generated/compile.h

  Kernel: arch/arm/boot/Image is ready

  SHIPPED arch/arm/boot/compressed/lib1funcs.S

  AS arch/arm/boot/compressed/lib1funcs.o

  LD arch/arm/boot/compressed/vmlinux

  OBJCOPY arch/arm/boot/zImage

  Kernel: arch/arm/boot/zImage is ready

  UIMAGE  arch/arm/boot/uImage

Image Name:   Linux-3.0.35+

Created:      Thu Jan 24 17:22:38 2013

Image Type:   ARM Linux Kernel Image (uncompressed)

Data Size:    3190904 Bytes = 3116.12 kB = 3.04 MB

Load Address: 0x00008000

Entry Point:  0x00008000

  Image arch/arm/boot/uImage is ready

+ grep -q ^CONFIG_MODULES= ./.config

+ make ARCH=arm CROSS_COMPILE= HOSTCC=ccache /usr/bin/gcc -B/usr/bin/ modules

  CHK include/linux/version.h

  CHK include/generated/utsrelease.h

make[1]: `include/generated/mach-types.h' is up to date.

  CALL scripts/checksyscalls.sh

  CC [M]  net/dccp/ccid.o

  CC [M] net/core/pktgen.o

  CC [M]  net/decnet/af_decnet.o

  CC [M]  net/dccp/feat.o

  CC [M]  net/dccp/input.o

  CC [M]  net/dccp/minisocks.o

net/core/pktgen.c: In function 'pktgen_if_show':

net/core/pktgen.c:682:2775: error: can't find a register in class 'GENERAL_REGS' while reloading 'asm'

net/core/pktgen.c:682:3153: error: can't find a register in class 'GENERAL_REGS' while reloading 'asm'

net/core/pktgen.c:682:2775: error: 'asm' operand has impossible constraints

net/core/pktgen.c:682:3153: error: 'asm' operand has impossible constraints

make[2]: *** [net/core/pktgen.o] Error 1

make[1]: *** [net/core] Error 2

make[1]: *** Waiting for unfinished jobs....

  CC [M] net/decnet/dn_nsp_in.o

  CC [M]  net/dccp/options.o

  CC [M]  net/dccp/output.o

  CC [M]  net/decnet/dn_nsp_out.o

  CC [M]  net/dccp/proto.o

  CC [M]  net/decnet/dn_route.o

  CC [M]  net/decnet/dn_dev.o

  CC [M] net/decnet/dn_neigh.o

  CC [M] net/decnet/dn_timer.o

  CC [M]  net/dccp/timer.o

  CC [M]  net/dccp/qpolicy.o

  CC [M]  net/decnet/sysctl_net_decnet.o

  CC [M]  net/decnet/netfilter/dn_rtmsg.o

  CC [M]  net/dccp/ccids/ccid2.o

  CC [M]  net/dccp/ackvec.o

  CC [M]  net/dccp/ccids/ccid3.o

  CC [M]  net/dccp/ccids/lib/tfrc.o

  CC [M] net/dccp/ccids/lib/tfrc_equation.o

  CC [M] net/dccp/ccids/lib/packet_history.o

  LD [M] net/decnet/decnet.o

  LD [M] drivers/scsi/scsi_tgt.o

  CC [M]  drivers/scsi/advansys.o

  CC [M] net/dccp/ccids/lib/loss_interval.o

  CC [M] net/dccp/sysctl.o

  CC [M]  net/dccp/diag.o

  CC [M] net/dccp/ipv4.o

drivers/scsi/advansys.c:72:2: warning: #warning this driver is still not properly converted to the DMA API [-Wcpp]

drivers/scsi/advansys.c: In function 'advansys_get_sense_buffer_dma':

drivers/scsi/advansys.c:8376:2: error: implicit declaration of function 'dma_cache_sync' [-Werror=implicit-function-declaration]

cc1: some warnings being treated as errors

make[2]: *** [drivers/scsi/advansys.o] Error 1

make[1]: *** [drivers/scsi] Error 2

make[1]: *** Waiting for unfinished jobs....

  CC [M] net/dccp/ipv6.o

  CC [M]  net/dccp/probe.o

make: *** [drivers] Error 2

make: *** Waiting for unfinished jobs....

net/dccp/probe.c: In function 'dccpprobe_init':

net/dccp/probe.c:166:53: warning: the omitted middle operand in ?: will always be 'true', suggest explicit middle operand [-Wparentheses]

  LD [M]  net/dccp/dccp.o

  LD [M]  net/dccp/dccp_ipv4.o

  LD [M]  net/dccp/dccp_ipv6.o

  LD [M] net/dccp/dccp_diag.o

  LD [M]  net/dccp/dccp_probe.o

make: *** [net] Error 2

error: Bad exit status from /home/dirk/projects/dcns/sabre/src/ltib/tmp/rpm-tmp.41639 (%build)

RPM build errors:

    Bad exit status from /home/dirk/projects/dcns/sabre/src/ltib/tmp/rpm-tmp.41639 (%build)

Build time for kernel-3.0.35: 205 seconds

Failed building kernel-3.0.35

f_buildrpms() returned an error, exiting

traceback:

main:572

Started: Thu Jan 24 17:21:10 2013

Ended:   Thu Jan 24 17:24:36 2013

Elapsed: 206 seconds

These packages failed to build:

kernel-3.0.35

Build Failed

Exiting on error or interrupt

dirk@dirk-desktop:~/projects/dcns/sabre/src/ltib$

标签 (3)
0 项奖励
回复
3 回复数

1,394 次查看
daiane_angolini
NXP Employee
NXP Employee

Every time I need to rebuild a kernel, I configure and build it manually.

export ARCH=arm

export CROSS_COMPILE=/opt/freescale/usr/toolchain/arm-eabi-4.4.3/bin/arm-eabi-

Pay attention ar arm-eabi version you have on your machine. Look for arm-eabi under /opt/freecale/usr and find your path

Then, enter your kernel dir:

$cd kernel_dir

$ ls arch/arm/config | grep -irn mx

here you will see *every* config file. Choose the right one for your board

$ make mx6config

$ make menuconfig

if you want to change any configuration

$make uImage

Please, make sure to use the right commands.

1,394 次查看
djbuijs
Contributor I

Thanks for your reply. This is the listing I get with def configs: there does not seem to be a imx6 default config....


dirk@dirk-desktop:~/projects/dcns/sabre/src/ltib$

ls rpm/BUILD/linux-3.0.35/arch/arm/configs/ | grep mx

mx1_defconfig

mx21_defconfig

mx27_defconfig

mx3_defconfig

mx51_defconfig

mxs_defconfig


Did I get the wrong source?


The source (L3.0.35_1.1.0_121218_source.tar.gz) was downloaded from https://www.freescale.com/webapp/Download?colCode=L3.0.35_1.1.0_SOURCE&appType=license&location=null...


Thanks,

Dirk


0 项奖励
回复

1,394 次查看
daiane_angolini
NXP Employee
NXP Employee

sorry for my delay.

I´m sure you have the right source code. But I´m not sure how your LTIB is configured.

Double check if you chose imx6 as your platform. If you need to reset every configuration, please, ./ltib -m selectype

You can also take the kernel source code from git repository:

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_3.0.35_1.1.0

by

git clone git://git.freescale.com/imx/linux-2.6-imx.git -b imx_3.0.35_1.1.0