timedatectl Not found in the systemd yocto Image

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

timedatectl Not found in the systemd yocto Image

5,764 次查看
devendrasinghba
Contributor II

Hi All,

I am using yocto tool-chain to build the custom Linux image ( systemd as init system). As I know timedatectl is installing as a part of the systemd_229.bb file but after including the systemd in my image .bb file, still I am not getting timedatectl command in the image. Anyone have any idea how to include timedatectl in the yocto image.

Thanks

标签 (3)
0 项奖励
回复
2 回复数

4,359 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi

Did you enable successfully the tymesync service?, the steps provided in previous thread work for you?:

https://community.nxp.com/thread/449974 

Regards

0 项奖励
回复

4,359 次查看
devendrasinghba
Contributor II

Hi,

To create service file "/lib/systemd/systemd-timesyncd" should come into the Linux image but this itself is not coming in the image. So my question is, how to add systemd-timesyncd and timedatectl in the yocto Image.

Below is the Terminal Log that will clarify what I want to say :

   root@imx6ulevk:/# find -name *systemd-timesyncd*
   root@imx6ulevk:/# find -name timedatectl
   root@imx6ulevk:/#

Thanks

0 项奖励
回复